Bootloader SDK for S32K148EVB-Q176

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bootloader SDK for S32K148EVB-Q176

Jump to solution
2,902 Views
Chandra13
Contributor I

Hello,

  1. Is there a bootloader SDK available for the S32K148? I tried Select Board | MCUXpresso SDK Builder (nxp.com), but I could not find the specific configuration.
  2. For now, I use the Design Studio 3.4 to work on other topics (SPI, CAN, LIN). Do I need to download the MCUXpresso IDE to work on the bootloader topics?
0 Kudos
Reply
1 Solution
2,893 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Chandra13

1. We do not provide such SDK to customers, only some application notes and demos, these demos are based on the old version of the SDK, and cannot be directly run on the new version of the IDE, such as S32 V3.4.

AN12218: S32K1xx Bootloader – Application Note  

AN12323: S32K1xx Firmware updates – Application Note  

Unified bootloader Demo 


2. MCUXpresso IDE has nothing to do with S32K.

View solution in original post

0 Kudos
Reply
2 Replies
2,894 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Chandra13

1. We do not provide such SDK to customers, only some application notes and demos, these demos are based on the old version of the SDK, and cannot be directly run on the new version of the IDE, such as S32 V3.4.

AN12218: S32K1xx Bootloader – Application Note  

AN12323: S32K1xx Firmware updates – Application Note  

Unified bootloader Demo 


2. MCUXpresso IDE has nothing to do with S32K.

0 Kudos
Reply
1,762 Views
CHYYDS
Contributor II

@Senlent Hello, do you have any information or documents related to bootloader for S32K344? Can you provide a link? Thank you very much!

0 Kudos
Reply