Linux Embedded Challenge ナレッジベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linux Embedded Challenge Knowledge Base

ラベル

ディスカッション

ソート順:
RS Lang Milestone 2: Build the controlling application Build an application that sets the speed of the car at a certain value. The car should be able to move with constant speed and when a new speed value is received from the app, it should accelerate or brake properly.
記事全体を表示
We implemented an application in c that helps us control the car. We are sending data between cores using serial transmision. We also started to implement a part of the bonus (change direction to avoid obstacles). The source code will be available on git.
記事全体を表示
The robot is assembled and powered from battery. User is able to command the robot wheels from the web interface.
記事全体を表示
Simple web interface for controlling our robot. It contains buttons for movement and a console for robot output.
記事全体を表示
we have implemented a web interface from where the user can: send  a hexadecimal code (the code must begin with "0x") to the board send a code and a date/time that will be scheduled get into learning mode and input names for the codes that will be received by the board
記事全体を表示
Am prezentat in video-ul atasat planul proiectului in linii mari,conexiunea intre udoo si computer, udoo si camera video, conexiunea la wifi si utilizarea VNC-ului.
記事全体を表示
Am instalat Tomcat 8.5.14 si MySQL server 5.5 pe placuta UdooNeo, apoi am realizat o aplicatie web in Tomcat care sa faca legatura intre o interfata grafica in browser accesabila de catre utilizator si baza de date. Utilizatorul poate cere in request pentru o anumita data, ora si durata iar daca nu mai exista in request in acea perioada de timp utilizatorul primeste in cod pe care il poate folosi pentru a accesa serverul in perioada de timp ceruta.
記事全体を表示
For this milestone, the new implemented functionality consists of: - adding login/logout feature - enabling an admin user to add new users - separating devices by users and commands by devices - adding IR learning functionality for devices which use the Sony protocol - lighting up a LED while the device is in learning mode
記事全体を表示
Buna ziua, Pentru primul milestone am conectat o pereche laser-fotorezistor la plăcuța UDOO și am citit valorile analogice (simuland inaltimea produsului final). Multumim !
記事全体を表示
We connected udoo to wireless Installed apache  We added some buttons to control the movement of the robot We had to put the web server on port 81 because we had some issues with apache and port 80
記事全体を表示
Am imbunatatit partea de transmisie seriala pentru a putea trimite si Ack inapoi la server-ul de python pentru a verifica ca datele au fost primite de catre partea de arduino. Am implementat scrierea de semnale PWM pe ESC-uri pentru a putea controla motoarele Am construit drona pentru a putea testa toate componentele si controlul motoarelor Am folosit Neo.Gpio pentru a lua datele de la senzori si a le avea pe server-ul python
記事全体を表示
A video showing the first few features of our Adaptive Headlights project. So far, we put together: power on/off buttons LEDs for the low beams, high beams and side lights servos for the high beams When the angle at which the wheel is tilted is greater than a certain threshold, the side lights are turned on progressively, in order to improve vision of the incoming portion of road. When the angle is lower than said threshold, the high beams adapt their position to follow the road.
記事全体を表示
   Realizarea primului milestone presupune realizarea interfetei web, care sa contina atat butoane pentru controlul robotului, cat si o fereastra de feedback de la acesta. Interfata este structurata astfel incat sa contina blocuri pentru: - status-ul de conectare; - live streaming; - feedback de la robot; - controlul robotului de la distanta.    Pentru realizarea interfetei si a comuncarii dintre interfata si Arduino, au fost necesare urmatoarele fisiere: - server.py (programul aflat in acest fisier este responsabil pentru crearea webserver-ului); - serialworker.py; - main.js; - index.html; - css.css; - serial2ws.ino.  
記事全体を表示
Am uploadat un scurt demo ce cuprinde o descrierea a: - algoritmului folosit. - modul de functionare.
記事全体を表示