ls1026a linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ls1026a linux

2,700 Views
renaud
Contributor IV

Hello,

we have a prototype using a LS1026A. We go tout boot loader booting and no are trying to boot Linux. The kernel we are using is running on the LS1046ardb eval board. 

Linux dies upon returning from  the init_el1 function.

Any clue why this would happen?

Cheers,

Renaud

 

 

Tags (3)
0 Kudos
Reply
4 Replies

2,628 Views
renaud
Contributor IV

. I used the PPA firmware from 2018 and Linux boots now.

0 Kudos
Reply

2,689 Views
renaud
Contributor IV
Returning from the function is when the "eret" instructions is run.
0 Kudos
Reply

2,691 Views
renaud
Contributor IV

Is that related to the use of the PPA firmware?

0 Kudos
Reply

2,660 Views
Oswalag
NXP TechSupport
NXP TechSupport

Hello, for newer versions of LSDK the TFA firmware (LSDK 18.12 onward) replaces PPA firmware (LSDK 18.09) as trusted firmware in U-Boot boot flow, please check what version you are using. 

0 Kudos
Reply