ls1026a linux

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ls1026a linux

2,695 次查看
renaud
Contributor IV

Hello,

we have a prototype using a LS1026A. We go tout boot loader booting and no are trying to boot Linux. The kernel we are using is running on the LS1046ardb eval board. 

Linux dies upon returning from  the init_el1 function.

Any clue why this would happen?

Cheers,

Renaud

 

 

标记 (3)
0 项奖励
回复
4 回复数

2,623 次查看
renaud
Contributor IV

. I used the PPA firmware from 2018 and Linux boots now.

0 项奖励
回复

2,684 次查看
renaud
Contributor IV
Returning from the function is when the "eret" instructions is run.
0 项奖励
回复

2,686 次查看
renaud
Contributor IV

Is that related to the use of the PPA firmware?

0 项奖励
回复

2,655 次查看
Oswalag
NXP TechSupport
NXP TechSupport

Hello, for newer versions of LSDK the TFA firmware (LSDK 18.12 onward) replaces PPA firmware (LSDK 18.09) as trusted firmware in U-Boot boot flow, please check what version you are using. 

0 项奖励
回复