USB Over Current Condition in LS1046

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Over Current Condition in LS1046

ソリューションへジャンプ
3,307件の閲覧回数
rashmikj
Contributor III

Hi

I am working on our custom board based on LS1046A Processor. 

The kernel log has "usb usb3-port1: over-current condition" and "usb usb4-port1: over-current condition" .   We are not using USB in our card and USB_PWRFAULT pin is connected to ground and  USB_DRVVBUS is left floating.

We even tried modifying this register "SCFG_USBPWRFAULT_SELCR "  with both 0x00000000 and 0x00000015(little-endian) But there is no change.

USB2_PWRFAULT,  USB3_PWRFAULT, USB2_DRVVBUS and USB3_DRVVBUS is used as GPIOs.

0 件の賞賛
返信
1 解決策
3,299件の閲覧回数
Pavel
NXP Employee
NXP Employee

Default configuration in u-boot for the SCFG_USBPWRFAULT_SELCR register is 0x2900_0000 (big-endian).

It means that USB1, USB2 and USB3 controllers receive PWRFAULT from dedicated USBx_PWRFAULT I/O.

The USB3_PWRFAULT signal is not used and this pin is assigned to TDMB_RQ. See the LS1043ARDB schematic.

 

Use the following command in u-boot:

mw 0x1570414 0x09000000

This command sets 0b00 for USB3:

00 - USB controller 3 has its PWRFAULT input tied inactive (no fault)

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,300件の閲覧回数
Pavel
NXP Employee
NXP Employee

Default configuration in u-boot for the SCFG_USBPWRFAULT_SELCR register is 0x2900_0000 (big-endian).

It means that USB1, USB2 and USB3 controllers receive PWRFAULT from dedicated USBx_PWRFAULT I/O.

The USB3_PWRFAULT signal is not used and this pin is assigned to TDMB_RQ. See the LS1043ARDB schematic.

 

Use the following command in u-boot:

mw 0x1570414 0x09000000

This command sets 0b00 for USB3:

00 - USB controller 3 has its PWRFAULT input tied inactive (no fault)

0 件の賞賛
返信