Recommended ULPI to USB IC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Recommended ULPI to USB IC

跳至解决方案
2,113 次查看
nicholashooper
Contributor II

Hi All,

Was looking to see is there was a recommended ULPI to USB device for the LS1012A.
I was originally looking at the USB3300, but I would like to see if there is something that has been used with the NXP processors

Many thanks in advance for your help.

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,978 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,

There is not any recommended ULPI USB device for the LS1012A. On the LS1012AQDS they implemented USB 2.0 using the nxp ISP1507B transceiver.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,979 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,

There is not any recommended ULPI USB device for the LS1012A. On the LS1012AQDS they implemented USB 2.0 using the nxp ISP1507B transceiver.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复