Recommended ULPI to USB IC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Recommended ULPI to USB IC

ソリューションへジャンプ
2,129件の閲覧回数
nicholashooper
Contributor II

Hi All,

Was looking to see is there was a recommended ULPI to USB device for the LS1012A.
I was originally looking at the USB3300, but I would like to see if there is something that has been used with the NXP processors

Many thanks in advance for your help.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,994件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

There is not any recommended ULPI USB device for the LS1012A. On the LS1012AQDS they implemented USB 2.0 using the nxp ISP1507B transceiver.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,995件の閲覧回数
r8070z
NXP Employee
NXP Employee


Have a great day,

There is not any recommended ULPI USB device for the LS1012A. On the LS1012AQDS they implemented USB 2.0 using the nxp ISP1507B transceiver.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信