Recommended ULPI to USB IC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Recommended ULPI to USB IC

Jump to solution
2,134 Views
nicholashooper
Contributor II

Hi All,

Was looking to see is there was a recommended ULPI to USB device for the LS1012A.
I was originally looking at the USB3300, but I would like to see if there is something that has been used with the NXP processors

Many thanks in advance for your help.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,999 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

There is not any recommended ULPI USB device for the LS1012A. On the LS1012AQDS they implemented USB 2.0 using the nxp ISP1507B transceiver.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,000 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

There is not any recommended ULPI USB device for the LS1012A. On the LS1012AQDS they implemented USB 2.0 using the nxp ISP1507B transceiver.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply