LS2085A CPU clock reconfiguration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS2085A CPU clock reconfiguration

ソリューションへジャンプ
3,110件の閲覧回数
anandhakumarm
Contributor III

I'm using LS2085A processor, in this 8 cpu cores are there, each one running at 1600 MHz, i want to change this into 1800 MHz.. Is there any way to change this by configuring RCW or u-boot ?

ラベル(1)
0 件の賞賛
返信
1 解決策
2,969件の閲覧回数
Bulat
NXP Employee
NXP Employee

Core's frequency is set up in the RCW, this is what you need to change.

Regards,

Bulat

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,970件の閲覧回数
Bulat
NXP Employee
NXP Employee

Core's frequency is set up in the RCW, this is what you need to change.

Regards,

Bulat

0 件の賞賛
返信
2,969件の閲覧回数
anandhakumarm
Contributor III

Meanwhile i also found the same. Anyway thank you so much for your valuable reply :smileyhappy:

0 件の賞賛
返信