LS1088a external interrupt in Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1088a external interrupt in Linux

2,432 Views
mrecoskie
Contributor III

Hi,

Does anyone have a working example of setting up an external (active low) interrupt to the ls1088a processor which they could share? I am writing a kernel module to handle interrupts and I have tried setting this up as a direct interrupt and as a GPIO through expander. I have also tried using the recent ‘extirq’ linux kernel changes added to v5.5. In all cases the processor does not recognize the interrupt assertion.

Any help is much appreciated. Thank you.

Mark

 

0 Kudos
Reply
1 Reply

2,396 Views
Pavel
NXP Employee
NXP Employee

Use sysfs for GPIO inputs.

This LSDK provides correct operation for sysfs using for GPIO inputs.

Use sysfs for using interrupt from the GPIO4_06.

See attached message dump for testing the GPIO4_06 input.

0 Kudos
Reply