the R764 on the J68 of the LS1088ARDB board root@TinyLinux:~# cat /sys/kernel/debug/gpio gpiochip3: GPIOs 384-415, parent: platform/2330000.gpio, 2330000.gpio: gpiochip2: GPIOs 416-447, parent: platform/2320000.gpio, 2320000.gpio: gpiochip1: GPIOs 448-479, parent: platform/2310000.gpio, 2310000.gpio: gpiochip0: GPIOs 480-511, parent: platform/2300000.gpio, 2300000.gpio: root@TinyLinux:~# cd .. root@TinyLinux:/home# cd .. root@TinyLinux:/# ls bin boot dev etc home init lib media mnt proc root run sbin sys tmp usr var root@TinyLinux:/# cd sys root@TinyLinux:/sys# cd class root@TinyLinux:/sys/class# ls ata_device devfreq hnae mem phy sas_end_device spi_master typec_mux vtconsole ata_link dma hwmon misc power_supply sas_expander spi_slave ubi wakeup ata_port drm i2c-adapter mmc_host pps sas_host spidev udc watchdog backlight dvb i2c-dev mtd ptp sas_phy tee uio bdi extcon input mux pwm sas_port thermal usb_role block firmware iommu net regulator scsi_device tpm vc bsg fpga_manager leds nvme remoteproc scsi_disk tpmrm vfio chromeos gpio macvtap nvme-subsystem rtc scsi_host tty video4linux devcoredump graphics mdio_bus pci_bus sas_device sound typec virtio-ports root@TinyLinux:/sys/class# cd gpio root@TinyLinux:/sys/class/gpio# echo 390 > export root@TinyLinux:/sys/class/gpio# cd gpio390 root@TinyLinux:/sys/class/gpio/gpio390# echo in > direction // input root@TinyLinux:/sys/class/gpio/gpio390# cat value 1 root@TinyLinux:/sys/class/gpio/gpio390# echo both > edge root@TinyLinux:/sys/class/gpio/gpio390# cd .. root@TinyLinux:/sys/class/gpio# more gpio390/* :::::::::::::: gpio390/active_low :::::::::::::: 0 :::::::::::::: gpio390/consumers :::::::::::::: *** gpio390/device: directory *** :::::::::::::: gpio390/direction :::::::::::::: in :::::::::::::: gpio390/edge :::::::::::::: both *** gpio390/power: directory *** *** gpio390/subsystem: directory *** :::::::::::::: gpio390/suppliers :::::::::::::: :::::::::::::: gpio390/uevent :::::::::::::: :::::::::::::: gpio390/value :::::::::::::: 1 root@TinyLinux:/sys/class/gpio# cd gpio390 root@TinyLinux:/sys/class/gpio/gpio390# cat value 1 root@TinyLinux:/sys/class/gpio/gpio390# cat value 0