LS1046 CW TAP:DDR validation Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1046 CW TAP:DDR validation Error

ソリューションへジャンプ
1,722件の閲覧回数
Hmc510
Contributor II

LS1046 DDR 8G . 1800MT

I modified the code in project ATF with ddrTfa_1.c 
DDR validation:

Hmc510_0-1670931326634.png

 

0 件の賞賛
返信
1 解決策
1,704件の閲覧回数
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @Hmc510,

There are few possible reasons for the error as mentioned below:

  1. The training sequence that the controller follows to calibrate the read data path was not able to complete. This would probably only happen if there was a hard failure on the memory interface caused by board-level issues or incorrect controller settings.
  1. Incorrect termination of MDICx signals.
  1. Write leveling calibration was not able to complete. This relates to improper settings of the DDR_WRLVL_CNTL register or board-level issues.

 

Regards,

Mrudang

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,705件の閲覧回数
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @Hmc510,

There are few possible reasons for the error as mentioned below:

  1. The training sequence that the controller follows to calibrate the read data path was not able to complete. This would probably only happen if there was a hard failure on the memory interface caused by board-level issues or incorrect controller settings.
  1. Incorrect termination of MDICx signals.
  1. Write leveling calibration was not able to complete. This relates to improper settings of the DDR_WRLVL_CNTL register or board-level issues.

 

Regards,

Mrudang

0 件の賞賛
返信