LS1046 CW TAP:DDR validation Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046 CW TAP:DDR validation Error

Jump to solution
1,724 Views
Hmc510
Contributor II

LS1046 DDR 8G . 1800MT

I modified the code in project ATF with ddrTfa_1.c 
DDR validation:

Hmc510_0-1670931326634.png

 

0 Kudos
Reply
1 Solution
1,706 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @Hmc510,

There are few possible reasons for the error as mentioned below:

  1. The training sequence that the controller follows to calibrate the read data path was not able to complete. This would probably only happen if there was a hard failure on the memory interface caused by board-level issues or incorrect controller settings.
  1. Incorrect termination of MDICx signals.
  1. Write leveling calibration was not able to complete. This relates to improper settings of the DDR_WRLVL_CNTL register or board-level issues.

 

Regards,

Mrudang

View solution in original post

0 Kudos
Reply
1 Reply
1,707 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @Hmc510,

There are few possible reasons for the error as mentioned below:

  1. The training sequence that the controller follows to calibrate the read data path was not able to complete. This would probably only happen if there was a hard failure on the memory interface caused by board-level issues or incorrect controller settings.
  1. Incorrect termination of MDICx signals.
  1. Write leveling calibration was not able to complete. This relates to improper settings of the DDR_WRLVL_CNTL register or board-level issues.

 

Regards,

Mrudang

0 Kudos
Reply