LS1046afrwy QSPI VFS error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1046afrwy QSPI VFS error

Jump to solution
2,632 Views
Autumn
Contributor II

Hi,

I am trying to boot a linux 5.15 from QSPI on the LS1046afrwy board.  I am getting the error, VFS: Cannot open root device "(null)" or unknown-block(0,0): error -6.

Below is the full output from the terminal.

NOTICE: Fixed DDR on board

NOTICE: 4 GB DDR4, 64-bit, CL=15, ECC on
NOTICE: BL2: v1.5(release):ls1046afrwy-early-access-bsp0.1
NOTICE: BL2: Built : 08:51:58, Dec 9 2022
NOTICE: BL31: v1.5(release):ls1046afrwy-early-access-bsp0.1
NOTICE: BL31: Built : 08:34:03, Dec 7 2022
NOTICE: Welcome to LS1046 BL31 Phase


U-Boot 2018.09 (Dec 07 2022 - 14:19:23 +0000)

SoC: LS1046AE Rev1.0 (0x87070010)
Clock Configuration:
CPU0(A72):1600 MHz CPU1(A72):1600 MHz CPU2(A72):1600 MHz
CPU3(A72):1600 MHz
Bus: 600 MHz DDR: 2100 MT/s FMAN: 700 MHz
Reset Configuration Word (RCW):
00000000: 0c150010 0e000000 00000000 00000000
00000010: 30400506 00800012 40025000 c1000000
00000020: 00000000 00000000 00000000 00038800
00000030: 20044100 24003101 00000096 00000001
Model: LS1046A FRWY Board
Board: LS1046AFRWY, Rev: A, boot from QSPI
SD1_CLK1 = 100.00MHZ, SD1_CLK2 = 100.00MHZ
I2C: ready
DRAM: 3.9 GiB (DDR4, 64-bit, CL=15, ECC on)
SEC0: RNG instantiated
Using SERDES1 Protocol: 12352 (0x3040)
Using SERDES2 Protocol: 1286 (0x506)
NAND: 512 MiB
MMC: FSL_SDHC: 0
Loading Environment from SPI Flash... SF: Detected mt25qu512a with page size 256 Bytes, erase size 64 KiB, total 64 MiB
*** Warning - bad CRC, using default environment

EEPROM: NXID v1
In: serial
Out: serial
Err: serial
Net: SF: Detected mt25qu512a with page size 256 Bytes, erase size 64 KiB, total 64 MiB
Fman1: Uploading microcode version 106.4.18
PCIe0: pcie@3400000 disabled
PCIe1: pcie@3500000 Root Complex: no link
PCIe2: pcie@3600000 Root Complex: no link
FM1@DTSEC1, FM1@DTSEC5, FM1@DTSEC6, FM1@DTSEC10
Hit any key to stop autoboot: 0
scanning bus for devices...

Device 0: unknown device
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:1...
starting USB...
USB0: Register 200017f NbrPorts 2
Starting the controller
USB XHCI 1.00
USB1: Register 200017f NbrPorts 2
Starting the controller
USB XHCI 1.00
USB2: Register 200017f NbrPorts 2
Starting the controller
USB XHCI 1.00
scanning bus 0 for devices... 1 USB Device(s) found
scanning bus 1 for devices... 1 USB Device(s) found
scanning bus 2 for devices... 1 USB Device(s) found
scanning usb for storage devices... 0 Storage Device(s) found

Device 0: unknown device
Trying load from qspi..
SF: Detected mt25qu512a with page size 256 Bytes, erase size 64 KiB, total 64 MiB
device 0 offset 0x1000000, size 0x2800000
SF: 41943040 bytes @ 0x1000000 Read: OK
## Loading kernel from FIT Image at a0000000 ...
Using 'ls1046afrwy' configuration
Trying 'kernel' kernel subimage
Description: ARM64 Kernel
Created: 2022-12-08 19:46:24 UTC
Type: Kernel Image
Compression: gzip compressed
Data Start: 0xa00000d0
Data Size: 10982175 Bytes = 10.5 MiB
Architecture: AArch64
OS: Linux
Load Address: 0x80080000
Entry Point: 0x80080000
Hash algo: crc32
Hash value: 251b8094
Verifying Hash Integrity ... crc32+ OK
## Loading fdt from FIT Image at a0000000 ...
Using 'ls1046afrwy' configuration
Trying 'ls1046afrwy-dtb' fdt subimage
Description: ls1046afrwy-dtb
Created: 2022-12-08 19:46:24 UTC
Type: Flat Device Tree
Compression: uncompressed
Data Start: 0xa0a794d4
Data Size: 31545 Bytes = 30.8 KiB
Architecture: AArch64
Load Address: 0x90000000
Hash algo: crc32
Hash value: 94a5427f
Verifying Hash Integrity ... crc32+ OK
Loading fdt from 0xa0a794d4 to 0x90000000
Booting using the fdt blob at 0x90000000
Uncompressing Kernel Image ... OK
Using Device Tree in place at 0000000090000000, end 000000009001ab38
WARNING failed to get smmu node: FDT_ERR_NOTFOUND
WARNING failed to get smmu node: FDT_ERR_NOTFOUND

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd082]
[ 0.000000] Linux version 5.15.72 (buildroot@buildroot) (aarch64-buildroot-linux-gnu-gcc.br_real (Buildroot rc-lts-2022.02.6-05) 11.3.0, GNU ld (GNU Binutils) 2.37) #1 SMP PREEMPT Thu Dec 8 13:46:24 CST 2022
[ 0.000000] Machine model: LS1046A FRWY Board
[ 0.000000] efi: UEFI not found.
[ 0.000000] [Firmware Bug]: Kernel image misaligned at boot, please fix your bootloader!
[ 0.000000] OF: reserved mem: initialized node bman-fbpr, compatible id fsl,bman-fbpr
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000080000000-0x00000008ffffffff]
[ 0.000000] NUMA: NODE_DATA [mem 0x8ff00bc00-0x8ff00dfff]
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal [mem 0x0000000100000000-0x00000008ffffffff]
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x00000000fbdfffff]
[ 0.000000] node 0: [mem 0x0000000880000000-0x00000008fbffffff]
[ 0.000000] node 0: [mem 0x00000008fc000000-0x00000008feffffff]
[ 0.000000] node 0: [mem 0x00000008ff000000-0x00000008ff7fffff]
[ 0.000000] node 0: [mem 0x00000008ff800000-0x00000008ffffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000008ffffffff]
[ 0.000000] On node 0, zone Normal: 16896 pages in unavailable ranges
[ 0.000000] cma: Reserved 32 MiB at 0x00000000f9c00000
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: MIGRATE_INFO_TYPE not supported.
[ 0.000000] psci: SMC Calling Convention v1.1
[ 0.000000] percpu: Embedded 20 pages/cpu s41304 r8192 d32424 u81920
[ 0.000000] Detected PIPT I-cache on CPU0
[ 0.000000] CPU features: detected: Spectre-v2
[ 0.000000] CPU features: detected: Spectre-v3a
[ 0.000000] CPU features: detected: Spectre-v4
[ 0.000000] CPU features: detected: Spectre-BHB
[ 0.000000] CPU features: kernel page table isolation forced ON by KASLR
[ 0.000000] CPU features: detected: Kernel page table isolation (KPTI)
[ 0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 1015296
[ 0.000000] Policy zone: Normal
[ 0.000000] Kernel command line:
[ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] software IO TLB: mapped [mem 0x00000000f5c00000-0x00000000f9c00000] (64MB)
[ 0.000000] Memory: 3864236K/4126720K available (15872K kernel code, 1264K rwdata, 5644K rodata, 2432K init, 471K bss, 229716K reserved, 32768K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GIC: Adjusting CPU interface base to 0x000000000142f000
[ 0.000000] Root IRQ handler: gic_handle_irq
[ 0.000000] GIC: Using split EOI/Deactivate mode
[ 0.000000] arch_timer: cp15 timer(s) running at 25.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x5c40939b5, max_idle_ns: 440795202646 ns
[ 0.000000] sched_clock: 56 bits at 25MHz, resolution 40ns, wraps every 4398046511100ns
[ 0.000132] Console: colour dummy device 80x25
[ 0.000306] printk: console [tty0] enabled
[ 0.000345] Calibrating delay loop (skipped), value calculated using timer frequency.. 50.00 BogoMIPS (lpj=100000)
[ 0.000356] pid_max: default: 32768 minimum: 301
[ 0.000385] LSM: Security Framework initializing
[ 0.000453] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.000484] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.001277] rcu: Hierarchical SRCU implementation.
[ 0.001461] EFI services will not be available.
[ 0.001576] smp: Bringing up secondary CPUs ...
[ 0.001837] Detected PIPT I-cache on CPU1
[ 0.001867] CPU1: Booted secondary processor 0x0000000001 [0x410fd082]
[ 0.002154] Detected PIPT I-cache on CPU2
[ 0.002172] CPU2: Booted secondary processor 0x0000000002 [0x410fd082]
[ 0.002445] Detected PIPT I-cache on CPU3
[ 0.002463] CPU3: Booted secondary processor 0x0000000003 [0x410fd082]
[ 0.002500] smp: Brought up 1 node, 4 CPUs
[ 0.002524] SMP: Total of 4 processors activated.
[ 0.002530] CPU features: detected: 32-bit EL0 Support
[ 0.002534] CPU features: detected: 32-bit EL1 Support
[ 0.002540] CPU features: detected: CRC32 instructions
[ 0.010847] CPU: All CPU(s) started at EL2
[ 0.010871] alternatives: patching kernel code
[ 0.011403] devtmpfs: initialized
[ 0.013511] KASLR enabled
[ 0.013579] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.013593] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[ 0.013998] DMI not present or invalid.
[ 0.014259] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[ 0.014849] DMA: preallocated 512 KiB GFP_KERNEL pool for atomic allocations
[ 0.014937] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.015054] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.015076] audit: initializing netlink subsys (disabled)
[ 0.015158] audit: type=2000 audit(0.012:1): state=initialized audit_enabled=0 res=1
[ 0.015377] thermal_sys: Registered thermal governor 'step_wise'
[ 0.015380] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.015625] cpuidle: using governor menu
[ 0.015665] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.015710] ASID allocator initialised with 32768 entries
[ 0.015777] Serial: AMBA PL011 UART driver
[ 0.020740] Machine: LS1046A FRWY Board
[ 0.020747] SoC family: QorIQ LS1046A
[ 0.020751] SoC ID: svr:0x87070010, Revision: 1.0
[ 0.031426] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.031439] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.031446] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.031452] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.032121] cryptd: max_cpu_qlen set to 1000
[ 0.033767] ACPI: Interpreter disabled.
[ 0.034660] iommu: Default domain type: Translated
[ 0.034668] iommu: DMA domain TLB invalidation policy: strict mode
[ 0.034733] vgaarb: loaded
[ 0.034843] SCSI subsystem initialized
[ 0.034991] usbcore: registered new interface driver usbfs
[ 0.035012] usbcore: registered new interface driver hub
[ 0.035029] usbcore: registered new device driver usb
[ 0.035324] imx-i2c 2180000.i2c: can't get pinctrl, bus recovery not supported
[ 0.035441] i2c i2c-0: IMX I2C adapter registered
[ 0.035465] i2c i2c-0: using dma0chan16 (tx) and dma0chan17 (rx) for DMA transfers
[ 0.035610] mc: Linux media interface: v0.10
[ 0.035624] videodev: Linux video capture interface: v2.00
[ 0.035658] pps_core: LinuxPPS API ver. 1 registered
[ 0.035664] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>
[ 0.035674] PTP clock support registered
[ 0.035693] EDAC MC: Ver: 3.0.0
[ 0.036026] fsl-ifc 1530000.ifc: Freescale Integrated Flash Controller
[ 0.036045] fsl-ifc 1530000.ifc: IFC version 1.4, 8 banks
[ 0.036170] FPGA manager framework
[ 0.036206] Advanced Linux Sound Architecture Driver Initialized.
[ 0.036420] Bluetooth: Core ver 2.22
[ 0.036436] NET: Registered PF_BLUETOOTH protocol family
[ 0.036442] Bluetooth: HCI device and connection manager initialized
[ 0.036449] Bluetooth: HCI socket layer initialized
[ 0.036454] Bluetooth: L2CAP socket layer initialized
[ 0.036463] Bluetooth: SCO socket layer initialized
[ 0.036567] clocksource: Switched to clocksource arch_sys_counter
[ 0.036650] VFS: Disk quotas dquot_6.6.0
[ 0.036676] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.036753] pnp: PnP ACPI: disabled
[ 0.039207] NET: Registered PF_INET protocol family
[ 0.039401] IP idents hash table entries: 65536 (order: 7, 524288 bytes, linear)
[ 0.040488] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes, linear)
[ 0.040508] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[ 0.040519] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 0.040594] TCP bind hash table entries: 32768 (order: 7, 524288 bytes, linear)
[ 0.040799] TCP: Hash tables configured (established 32768 bind 32768)
[ 0.040867] UDP hash table entries: 2048 (order: 4, 65536 bytes, linear)
[ 0.040889] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes, linear)
[ 0.040964] NET: Registered PF_UNIX/PF_LOCAL protocol family
[ 0.041149] RPC: Registered named UNIX socket transport module.
[ 0.041156] RPC: Registered udp transport module.
[ 0.041161] RPC: Registered tcp transport module.
[ 0.041165] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.041410] PCI: CLS 0 bytes, default 64
[ 0.041729] hw perfevents: enabled with armv8_cortex_a72 PMU driver, 7 counters available
[ 0.042036] kvm [1]: IPA Size Limit: 44 bits
[ 0.042471] kvm [1]: vgic interrupt IRQ9
[ 0.042541] kvm [1]: Hyp mode initialized successfully
[ 0.044242] Initialise system trusted keyrings
[ 0.044319] workingset: timestamp_bits=42 max_order=20 bucket_order=0
[ 0.047131] NFS: Registering the id_resolver key type
[ 0.047148] Key type id_resolver registered
[ 0.047153] Key type id_legacy registered
[ 0.047189] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.047196] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 0.047202] Installing knfsd (copyright (C) 1996 [email protected]).
[ 0.047260] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[ 0.047422] 9p: Installing v9fs 9p2000 file system support
[ 0.071776] Key type asymmetric registered
[ 0.071782] Asymmetric key parser 'x509' registered
[ 0.071809] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
[ 0.071817] io scheduler mq-deadline registered
[ 0.071822] io scheduler kyber registered
[ 0.073863] layerscape-pcie 3500000.pcie: host bridge /soc/pcie@3500000 ranges:
[ 0.073886] layerscape-pcie 3500000.pcie: IO 0x4800010000..0x480001ffff -> 0x0000000000
[ 0.073902] layerscape-pcie 3500000.pcie: MEM 0x4840000000..0x487fffffff -> 0x0040000000
[ 0.073932] layerscape-pcie 3500000.pcie: iATU unroll: disabled
[ 0.073938] layerscape-pcie 3500000.pcie: Detected iATU regions: 8 outbound, 6 inbound
[ 1.074012] layerscape-pcie 3500000.pcie: Phy link never came up
[ 1.074068] layerscape-pcie 3500000.pcie: PCI host bridge to bus 0000:00
[ 1.074076] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 1.074084] pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
[ 1.074091] pci_bus 0000:00: root bus resource [mem 0x4840000000-0x487fffffff] (bus address [0x40000000-0x7fffffff])
[ 1.074115] pci 0000:00:00.0: [1957:81c0] type 01 class 0x060400
[ 1.074133] pci 0000:00:00.0: reg 0x38: [mem 0x4840000000-0x48400007ff pref]
[ 1.074170] pci 0000:00:00.0: supports D1 D2
[ 1.074176] pci 0000:00:00.0: PME# supported from D0 D1 D2 D3hot
[ 1.075853] pci 0000:00:00.0: BAR 6: assigned [mem 0x4840000000-0x48400007ff pref]
[ 1.075865] pci 0000:00:00.0: PCI bridge to [bus 01-ff]
[ 1.075964] pcieport 0000:00:00.0: PME: Signaling with IRQ 81
[ 1.076085] layerscape-pcie 3600000.pcie: host bridge /soc/pcie@3600000 ranges:
[ 1.076106] layerscape-pcie 3600000.pcie: IO 0x5000010000..0x500001ffff -> 0x0000000000
[ 1.076119] layerscape-pcie 3600000.pcie: MEM 0x5040000000..0x507fffffff -> 0x0040000000
[ 1.076147] layerscape-pcie 3600000.pcie: iATU unroll: disabled
[ 1.076153] layerscape-pcie 3600000.pcie: Detected iATU regions: 8 outbound, 6 inbound
[ 2.076226] layerscape-pcie 3600000.pcie: Phy link never came up
[ 2.076269] layerscape-pcie 3600000.pcie: PCI host bridge to bus 0001:00
[ 2.076277] pci_bus 0001:00: root bus resource [bus 00-ff]
[ 2.076284] pci_bus 0001:00: root bus resource [io 0x10000-0x1ffff] (bus address [0x0000-0xffff])
[ 2.076293] pci_bus 0001:00: root bus resource [mem 0x5040000000-0x507fffffff] (bus address [0x40000000-0x7fffffff])
[ 2.076311] pci 0001:00:00.0: [1957:81c0] type 01 class 0x060400
[ 2.076328] pci 0001:00:00.0: reg 0x38: [mem 0x5040000000-0x50400007ff pref]
[ 2.076362] pci 0001:00:00.0: supports D1 D2
[ 2.076368] pci 0001:00:00.0: PME# supported from D0 D1 D2 D3hot
[ 2.078009] pci 0001:00:00.0: BAR 6: assigned [mem 0x5040000000-0x50400007ff pref]
[ 2.078020] pci 0001:00:00.0: PCI bridge to [bus 01-ff]
[ 2.078107] pcieport 0001:00:00.0: PME: Signaling with IRQ 82
[ 2.078706] EINJ: ACPI disabled.
[ 2.086385] bman_portal 508000000.bman-portal: Portal initialised, cpu 0
[ 2.086449] bman_portal 508010000.bman-portal: Portal initialised, cpu 1
[ 2.086501] bman_portal 508020000.bman-portal: Portal initialised, cpu 2
[ 2.086552] bman_portal 508030000.bman-portal: Portal initialised, cpu 3
[ 2.086846] qman_portal 500000000.qman-portal: Portal initialised, cpu 0
[ 2.086900] qman_portal 500010000.qman-portal: Portal initialised, cpu 1
[ 2.086951] qman_portal 500020000.qman-portal: Portal initialised, cpu 2
[ 2.087363] qman_portal 500030000.qman-portal: Portal initialised, cpu 3
[ 2.089016] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 2.089847] 21c0500.serial: ttyS0 at MMIO 0x21c0500 (irq = 46, base_baud = 18750000) is a 16550A
[ 3.376234] printk: console [ttyS0] enabled
[ 3.380660] 21c0600.serial: ttyS1 at MMIO 0x21c0600 (irq = 46, base_baud = 18750000) is a 16550A
[ 3.389677] 21d0500.serial: ttyS2 at MMIO 0x21d0500 (irq = 47, base_baud = 18750000) is a 16550A
[ 3.398698] 21d0600.serial: ttyS3 at MMIO 0x21d0600 (irq = 47, base_baud = 18750000) is a 16550A
[ 3.412520] loop: module loaded
[ 3.415976] megasas: 07.717.02.00-rc1
[ 3.420582] ahci-qoriq 3200000.sata: AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl platform mode
[ 3.429557] ahci-qoriq 3200000.sata: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc sds apst
[ 3.439563] scsi host0: ahci-qoriq
[ 3.443076] ata1: SATA max UDMA/133 mmio [mem 0x03200000-0x0320ffff] port 0x100 irq 58
[ 3.451757] nand: device found, Manufacturer ID: 0x01, Chip ID: 0xac
[ 3.458120] nand: AMD/Spansion S34MS04G2
[ 3.462043] nand: 512 MiB, SLC, erase size: 128 KiB, page size: 2048, OOB size: 128
[ 3.470215] Bad block table found at page 262080, version 0x01
[ 3.477010] Bad block table found at page 262016, version 0x01
[ 3.483879] fsl,ifc-nand 7e800000.nand: IFC NAND device at 0x7e800000, bank 0
[ 3.491661] spi-nor spi0.0: found mt25qu512a, expected m25p80
[ 3.497591] spi-nor spi0.0: mt25qu512a (65536 Kbytes)
[ 3.504331] tun: Universal TUN/TAP device driver, 1.6
[ 3.509809] thunder_xcv, ver 1.0
[ 3.513055] thunder_bgx, ver 1.0
[ 3.516294] nicpf, ver 1.0
[ 3.541200] fsl_dpaa_mac 1ae0000.ethernet: FMan MEMAC
[ 3.546263] fsl_dpaa_mac 1ae0000.ethernet: FMan MAC address: 00:04:9f:07:90:b3
[ 3.553831] fsl_dpaa_mac 1ae8000.ethernet: FMan MEMAC
[ 3.558889] fsl_dpaa_mac 1ae8000.ethernet: FMan MAC address: 00:04:9f:07:90:b4
[ 3.566435] fsl_dpaa_mac 1aea000.ethernet: FMan MEMAC
[ 3.571493] fsl_dpaa_mac 1aea000.ethernet: FMan MAC address: 00:04:9f:07:90:b5
[ 3.579038] fsl_dpaa_mac 1af2000.ethernet: FMan MEMAC
[ 3.584095] fsl_dpaa_mac 1af2000.ethernet: FMan MAC address: 00:04:9f:07:90:b6
[ 3.608633] fsl_dpaa_mac 1ae0000.ethernet eth0: Probed interface eth0
[ 3.632706] fsl_dpaa_mac 1ae8000.ethernet eth1: Probed interface eth1
[ 3.656966] fsl_dpaa_mac 1aea000.ethernet eth2: Probed interface eth2
[ 3.681498] fsl_dpaa_mac 1af2000.ethernet eth3: Probed interface eth3
[ 3.688603] hclge is initializing
[ 3.691922] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[ 3.699150] hns3: Copyright (c) 2017 Huawei Corporation.
[ 3.704485] e1000: Intel(R) PRO/1000 Network Driver
[ 3.709366] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 3.715131] e1000e: Intel(R) PRO/1000 Network Driver
[ 3.720103] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 3.726045] igb: Intel(R) Gigabit Ethernet Network Driver
[ 3.731447] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 3.737035] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[ 3.743305] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 3.749243] sky2: driver version 1.30
[ 3.753175] VFIO - User Level meta-driver version: 0.3
[ 3.759659] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 3.762743] ata1: SATA link down (SStatus 0 SControl 300)
[ 3.766200] ehci-pci: EHCI PCI platform driver
[ 3.776053] ehci-platform: EHCI generic platform driver
[ 3.781385] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 3.787573] ohci-pci: OHCI PCI platform driver
[ 3.792031] ohci-platform: OHCI generic platform driver
[ 3.797601] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 3.803100] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
[ 3.810852] xhci-hcd xhci-hcd.0.auto: hcc params 0x0220f66d hci version 0x100 quirks 0x0000002002010810
[ 3.820278] xhci-hcd xhci-hcd.0.auto: irq 55, io mem 0x02f00000
[ 3.826273] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[ 3.831765] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
[ 3.839432] xhci-hcd xhci-hcd.0.auto: Host supports USB 3.0 SuperSpeed
[ 3.846198] hub 1-0:1.0: USB hub found
[ 3.849960] hub 1-0:1.0: 1 port detected
[ 3.854200] hub 2-0:1.0: USB hub found
[ 3.857962] hub 2-0:1.0: 1 port detected
[ 3.862033] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 3.867528] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 3
[ 3.875265] xhci-hcd xhci-hcd.1.auto: hcc params 0x0220f66d hci version 0x100 quirks 0x0000002002010810
[ 3.884685] xhci-hcd xhci-hcd.1.auto: irq 56, io mem 0x03000000
[ 3.890679] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 3.896171] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 4
[ 3.903836] xhci-hcd xhci-hcd.1.auto: Host supports USB 3.0 SuperSpeed
[ 3.910552] hub 3-0:1.0: USB hub found
[ 3.914314] hub 3-0:1.0: 1 port detected
[ 3.918541] hub 4-0:1.0: USB hub found
[ 3.922306] hub 4-0:1.0: 1 port detected
[ 3.926373] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller
[ 3.931868] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 5
[ 3.939600] xhci-hcd xhci-hcd.2.auto: hcc params 0x0220f66d hci version 0x100 quirks 0x0000002002010810
[ 3.949020] xhci-hcd xhci-hcd.2.auto: irq 57, io mem 0x03100000
[ 3.955004] xhci-hcd xhci-hcd.2.auto: xHCI Host Controller
[ 3.960498] xhci-hcd xhci-hcd.2.auto: new USB bus registered, assigned bus number 6
[ 3.968165] xhci-hcd xhci-hcd.2.auto: Host supports USB 3.0 SuperSpeed
[ 3.974898] hub 5-0:1.0: USB hub found
[ 3.978658] hub 5-0:1.0: 1 port detected
[ 3.982880] hub 6-0:1.0: USB hub found
[ 3.986642] hub 6-0:1.0: 1 port detected
[ 3.990758] usbcore: registered new interface driver uas
[ 3.996115] usbcore: registered new interface driver usb-storage
[ 4.003513] ftm-alarm 29d0000.ftm0: registered as rtc0
[ 4.008666] ftm-alarm 29d0000.ftm0: setting system clock to 1970-01-01T00:00:04 UTC (4)
[ 4.016887] i2c_dev: i2c /dev entries driver
[ 4.022368] i2c i2c-0: Added multiplexed i2c bus 1
[ 4.027239] i2c i2c-0: Added multiplexed i2c bus 2
[ 4.032118] i2c i2c-0: Added multiplexed i2c bus 3
[ 4.036990] i2c i2c-0: Added multiplexed i2c bus 4
[ 4.041787] pca954x 0-0077: registered 4 multiplexed busses for I2C switch pca9546
[ 4.049577] ptp_qoriq: device tree node missing required elements, try automatic configuration
[ 4.058259] pps pps0: new PPS source ptp0
[ 4.078805] Bluetooth: HCI UART driver ver 2.3
[ 4.083255] Bluetooth: HCI UART protocol H4 registered
[ 4.088396] Bluetooth: HCI UART protocol BCSP registered
[ 4.093723] Bluetooth: HCI UART protocol LL registered
[ 4.098867] Bluetooth: HCI UART protocol ATH3K registered
[ 4.104276] Bluetooth: HCI UART protocol Three-wire (H5) registered
[ 4.110595] Bluetooth: HCI UART protocol Broadcom registered
[ 4.116265] Bluetooth: HCI UART protocol QCA registered
[ 4.121895] qoriq-cpufreq qoriq-cpufreq: Freescale QorIQ CPU frequency scaling driver
[ 4.130163] sdhci: Secure Digital Host Controller Interface driver
[ 4.136349] sdhci: Copyright(c) Pierre Ossman
[ 4.140941] Synopsys Designware Multimedia Card Interface Driver
[ 4.147326] sdhci-pltfm: SDHCI platform and OF driver helper
[ 4.153818] ledtrig-cpu: registered to indicate activity on CPUs
[ 4.160286] usbcore: registered new interface driver usbhid
[ 4.165867] usbhid: USB HID core driver
[ 4.170654] cs_system_cfg: CoreSight Configuration manager initialised
[ 4.176613] mmc0: SDHCI controller on 1560000.esdhc [1560000.esdhc] using ADMA 64-bit
[ 4.177548] optee: probing for conduit method.
[ 4.189552] optee: api uid mismatch
[ 4.193043] optee: probe of firmware:optee failed with error -22
[ 4.200236] NET: Registered PF_LLC protocol family
[ 4.205271] NET: Registered PF_INET6 protocol family
[ 4.210727] Segment Routing with IPv6
[ 4.214412] In-situ OAM (IOAM) with IPv6
[ 4.218360] NET: Registered PF_PACKET protocol family
[ 4.221256] mmc0: new high speed SDHC card at address aaaa
[ 4.223478] Bluetooth: RFCOMM TTY layer initialized
[ 4.229163] mmcblk0: mmc0:aaaa SL16G 14.8 GiB
[ 4.233788] Bluetooth: RFCOMM socket layer initialized
[ 4.243381] Bluetooth: RFCOMM ver 1.11
[ 4.244217] mmcblk0: p1
[ 4.247136] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 4.254977] Bluetooth: BNEP filters: protocol multicast
[ 4.260206] Bluetooth: BNEP socket layer initialized
[ 4.265171] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 4.271097] Bluetooth: HIDP socket layer initialized
[ 4.276079] lib80211: common routines for IEEE802.11 drivers
[ 4.281798] 9pnet: Installing 9P2000 support
[ 4.286100] Key type dns_resolver registered
[ 4.290450] Loading compiled-in X.509 certificates
[ 4.297817] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 4.306333] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 4.312910] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[ 4.316595] ALSA device list:
[ 4.321537] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db
[ 4.324543] No soundcards found.
[ 4.335914] VFS: Cannot open root device "(null)" or unknown-block(0,0): error -6
[ 4.344417] Please append a correct "root=" boot option; here are the available partitions:
[ 4.352785] 1f00 524288 mtdblock0
[ 4.352789] (driver?)
[ 4.359327] 1f01 65536 mtdblock1
[ 4.359330] (driver?)
[ 4.365868] b300 15558144 mmcblk0
[ 4.365872] driver: mmcblk
[ 4.372711] b301 15554048 mmcblk0p1 00000000-01
[ 4.372715]
[ 4.379517] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)
[ 4.387785] CPU: 3 PID: 1 Comm: swapper/0 Not tainted 5.15.72 #1
[ 4.393793] Hardware name: LS1046A FRWY Board (DT)
[ 4.398582] Call trace:
[ 4.401022] dump_backtrace+0x0/0x1a0
[ 4.404690] show_stack+0x18/0x70
[ 4.408002] dump_stack_lvl+0x68/0x84
[ 4.411664] dump_stack+0x18/0x34
[ 4.414975] panic+0x15c/0x31c
[ 4.418025] mount_block_root+0x17c/0x22c
[ 4.422034] mount_root+0x204/0x240
[ 4.425519] prepare_namespace+0x130/0x170
[ 4.429613] kernel_init_freeable+0x24c/0x290
[ 4.433968] kernel_init+0x24/0x130
[ 4.437454] ret_from_fork+0x10/0x20
[ 4.441028] SMP: stopping secondary CPUs
[ 4.444954] Kernel Offset: 0x1a4f080000 from 0xffffffc008000000
[ 4.450872] PHYS_OFFSET: 0x80000000
[ 4.454356] CPU features: 0x400004f1,00000846
[ 4.458709] Memory Limit: none
[ 4.461761] ---[ end Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0) ]---

Thank you.

0 Kudos
Reply
1 Solution
2,611 Views
Autumn
Contributor II

I resolved the issue by updating the *.its file.  My initrd configuration was incorrect.  

View solution in original post

0 Kudos
Reply
1 Reply
2,612 Views
Autumn
Contributor II

I resolved the issue by updating the *.its file.  My initrd configuration was incorrect.  

0 Kudos
Reply