How do I debug the LS1043ARDB's u-boot?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I debug the LS1043ARDB's u-boot?

ソリューションへジャンプ
3,461件の閲覧回数
ts1234
Contributor III

How do I debug the LS1043ARDB's u-boot?

0 件の賞賛
返信
1 解決策
3,459件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please refer to the CodeWarrior Development Studio for QorIQ LS series - ARM V8 ISA, Targeting Manual, 8.1 U-Boot debug or follow the section "Debug u-boot with CodeWarrior for ARMv8" in the step by step document (https://community.nxp.com/docs/DOC-331981) to debug u-boot with the Attach method:

元の投稿で解決策を見る

4 返答(返信)
3,451件の閲覧回数
ts1234
Contributor III

Does it support debugging with the DSTREAM Gen-1 debugger as well?

0 件の賞賛
返信
3,453件の閲覧回数
ts1234
Contributor III

Do I need to purchase some hardware as well? If yes, please share the link to go through the debugger purchase+licensing options.

0 件の賞賛
返信
3,448件の閲覧回数
ufedor
NXP Employee
NXP Employee

Tools supported by NXP:

1) Software - CodeWarrior IDE:

https://www.nxp.com/design/software/development-software/codewarrior-development-tools/codewarrior-n...

2) Hardware - CodeWarrior TAP Base Unit (CWH-CTP-BASE-HE) + Probe tip (CWH-CTP-CTX10-YE)

3,460件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please refer to the CodeWarrior Development Studio for QorIQ LS series - ARM V8 ISA, Targeting Manual, 8.1 U-Boot debug or follow the section "Debug u-boot with CodeWarrior for ARMv8" in the step by step document (https://community.nxp.com/docs/DOC-331981) to debug u-boot with the Attach method: