How do I debug the LS1043ARDB's u-boot?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I debug the LS1043ARDB's u-boot?

Jump to solution
3,652 Views
ts1234
Contributor III

How do I debug the LS1043ARDB's u-boot?

0 Kudos
Reply
1 Solution
3,650 Views
ufedor
NXP Employee
NXP Employee

Please refer to the CodeWarrior Development Studio for QorIQ LS series - ARM V8 ISA, Targeting Manual, 8.1 U-Boot debug or follow the section "Debug u-boot with CodeWarrior for ARMv8" in the step by step document (https://community.nxp.com/docs/DOC-331981) to debug u-boot with the Attach method:

View solution in original post

4 Replies
3,642 Views
ts1234
Contributor III

Does it support debugging with the DSTREAM Gen-1 debugger as well?

0 Kudos
Reply
3,644 Views
ts1234
Contributor III

Do I need to purchase some hardware as well? If yes, please share the link to go through the debugger purchase+licensing options.

0 Kudos
Reply
3,639 Views
ufedor
NXP Employee
NXP Employee

Tools supported by NXP:

1) Software - CodeWarrior IDE:

https://www.nxp.com/design/software/development-software/codewarrior-development-tools/codewarrior-n...

2) Hardware - CodeWarrior TAP Base Unit (CWH-CTP-BASE-HE) + Probe tip (CWH-CTP-CTX10-YE)

3,651 Views
ufedor
NXP Employee
NXP Employee

Please refer to the CodeWarrior Development Studio for QorIQ LS series - ARM V8 ISA, Targeting Manual, 8.1 U-Boot debug or follow the section "Debug u-boot with CodeWarrior for ARMv8" in the step by step document (https://community.nxp.com/docs/DOC-331981) to debug u-boot with the Attach method: