How do I debug the LS1043ARDB's u-boot?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How do I debug the LS1043ARDB's u-boot?

跳至解决方案
3,662 次查看
ts1234
Contributor III

How do I debug the LS1043ARDB's u-boot?

0 项奖励
回复
1 解答
3,660 次查看
ufedor
NXP Employee
NXP Employee

Please refer to the CodeWarrior Development Studio for QorIQ LS series - ARM V8 ISA, Targeting Manual, 8.1 U-Boot debug or follow the section "Debug u-boot with CodeWarrior for ARMv8" in the step by step document (https://community.nxp.com/docs/DOC-331981) to debug u-boot with the Attach method:

在原帖中查看解决方案

4 回复数
3,652 次查看
ts1234
Contributor III

Does it support debugging with the DSTREAM Gen-1 debugger as well?

0 项奖励
回复
3,654 次查看
ts1234
Contributor III

Do I need to purchase some hardware as well? If yes, please share the link to go through the debugger purchase+licensing options.

0 项奖励
回复
3,649 次查看
ufedor
NXP Employee
NXP Employee

Tools supported by NXP:

1) Software - CodeWarrior IDE:

https://www.nxp.com/design/software/development-software/codewarrior-development-tools/codewarrior-n...

2) Hardware - CodeWarrior TAP Base Unit (CWH-CTP-BASE-HE) + Probe tip (CWH-CTP-CTX10-YE)

3,661 次查看
ufedor
NXP Employee
NXP Employee

Please refer to the CodeWarrior Development Studio for QorIQ LS series - ARM V8 ISA, Targeting Manual, 8.1 U-Boot debug or follow the section "Debug u-boot with CodeWarrior for ARMv8" in the step by step document (https://community.nxp.com/docs/DOC-331981) to debug u-boot with the Attach method: