Loading the uboot and kernel from the SPI NOR flash on the LS1043A based custom board?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Loading the uboot and kernel from the SPI NOR flash on the LS1043A based custom board?

1,718 次查看
ts1234
Contributor III

How do I load the uboot and kernel from the SPI NOR flash on the LS1043 based custom board?

(Assuming that the SPI Flash MTD driver is already present in the kernel and uboot).

0 项奖励
回复
1 回复

1,713 次查看
ufedor
NXP Employee
NXP Employee

It is needed to build composite firmware image (1) and program it into the SPI Flash (2) - refer to the Layerscape SDK Documentation:

1) https://docs.nxp.com/bundle/GUID-3FFCCD77-5220-414D-8664-09E6FB1B02C6/page/GUID-EB58F77F-97D9-459A-A...

2) https://docs.nxp.com/bundle/GUID-3FFCCD77-5220-414D-8664-09E6FB1B02C6/page/GUID-DCD3FA8A-CA37-4DCF-B...

 

0 项奖励
回复