Does Data Path Acceleration work with PCIe-connected Ethernet Controllers?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Does Data Path Acceleration work with PCIe-connected Ethernet Controllers?

跳至解决方案
1,356 次查看
neil_weinstock
Contributor III

We're using the LS1043A in a product where high TCP throughput over 2.5 G ethernet is top priority.  Using the internal ethernet controllers, performance is great due to the data path acceleration.

Is the data path acceleration available if we were to use an external ethernet controller connected via PCIe, or is it sort of hard-wired to the internal controllers?  That is, could we expect similar levels of throughput with a PCIe-connected ethernet controller?

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,270 次查看
ufedor
NXP Employee
NXP Employee

The data path acceleration is available only for the SOC Ethernet modules.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,271 次查看
ufedor
NXP Employee
NXP Employee

The data path acceleration is available only for the SOC Ethernet modules.

0 项奖励
回复