Does Data Path Acceleration work with PCIe-connected Ethernet Controllers?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does Data Path Acceleration work with PCIe-connected Ethernet Controllers?

Jump to solution
1,789 Views
neil_weinstock
Contributor III

We're using the LS1043A in a product where high TCP throughput over 2.5 G ethernet is top priority.  Using the internal ethernet controllers, performance is great due to the data path acceleration.

Is the data path acceleration available if we were to use an external ethernet controller connected via PCIe, or is it sort of hard-wired to the internal controllers?  That is, could we expect similar levels of throughput with a PCIe-connected ethernet controller?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,703 Views
ufedor
NXP Employee
NXP Employee

The data path acceleration is available only for the SOC Ethernet modules.

View solution in original post

0 Kudos
Reply
1 Reply
1,704 Views
ufedor
NXP Employee
NXP Employee

The data path acceleration is available only for the SOC Ethernet modules.

0 Kudos
Reply