Does Data Path Acceleration work with PCIe-connected Ethernet Controllers?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does Data Path Acceleration work with PCIe-connected Ethernet Controllers?

ソリューションへジャンプ
1,779件の閲覧回数
neil_weinstock
Contributor III

We're using the LS1043A in a product where high TCP throughput over 2.5 G ethernet is top priority.  Using the internal ethernet controllers, performance is great due to the data path acceleration.

Is the data path acceleration available if we were to use an external ethernet controller connected via PCIe, or is it sort of hard-wired to the internal controllers?  That is, could we expect similar levels of throughput with a PCIe-connected ethernet controller?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,693件の閲覧回数
ufedor
NXP Employee
NXP Employee

The data path acceleration is available only for the SOC Ethernet modules.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,694件の閲覧回数
ufedor
NXP Employee
NXP Employee

The data path acceleration is available only for the SOC Ethernet modules.

0 件の賞賛
返信