lpc54018 Regarding the placement of the API Function Table

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpc54018 Regarding the placement of the API Function Table

Jump to solution
1,640 Views
yo_ku_
Contributor II

I'm not sure if this is a feature that is rarely used.
Is "LPC54S018M.h" wrong?

According to the specification, RESERVED_0 (= Ptr to DeviceTable) is 12 words.

Source.png

 

Manual.png

 B.R.

0 Kudos
Reply
1 Solution
1,624 Views
yo_ku_
Contributor II

Sorry.
I was able to confirm that RNG_GetRandomData() (it uses the OTP_API) works on RESERVED_0[13].
Perhaps the specification is wrong.

View solution in original post

0 Kudos
Reply
1 Reply
1,625 Views
yo_ku_
Contributor II

Sorry.
I was able to confirm that RNG_GetRandomData() (it uses the OTP_API) works on RESERVED_0[13].
Perhaps the specification is wrong.

0 Kudos
Reply