lpc54018 Regarding the placement of the API Function Table

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpc54018 Regarding the placement of the API Function Table

ソリューションへジャンプ
1,646件の閲覧回数
yo_ku_
Contributor II

I'm not sure if this is a feature that is rarely used.
Is "LPC54S018M.h" wrong?

According to the specification, RESERVED_0 (= Ptr to DeviceTable) is 12 words.

Source.png

 

Manual.png

 B.R.

0 件の賞賛
返信
1 解決策
1,630件の閲覧回数
yo_ku_
Contributor II

Sorry.
I was able to confirm that RNG_GetRandomData() (it uses the OTP_API) works on RESERVED_0[13].
Perhaps the specification is wrong.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,631件の閲覧回数
yo_ku_
Contributor II

Sorry.
I was able to confirm that RNG_GetRandomData() (it uses the OTP_API) works on RESERVED_0[13].
Perhaps the specification is wrong.

0 件の賞賛
返信