Which is the highest resolution supported by LPC54018 MCU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Which is the highest resolution supported by LPC54018 MCU

跳至解决方案
1,141 次查看
oscarniño
Contributor III

Hi I want to know which is de highest resolution supported by LPC54018, right now I'm working with 480x272 resolution display touch, but I need to use a 7' display, some body could tell me?

Best regards

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,083 次查看
Sabina_Bruce
NXP Employee
NXP Employee

Hi Oscar, 

The LCD Controller supports both Super-Twisted Nematic (STN) and Thin-Film Transistor (TFT) displays. It has a dedicated DMA controller, selectable display resolution (up to 1024 x 768 pixels), and supports up to 24-bit true-color mode.

For more information regarding the selectable display resolution you can refer to the LPC540xx/LPC54S0xx Data Sheet.

Let me know if this helps!

Sabina

在原帖中查看解决方案

2 回复数
1,084 次查看
Sabina_Bruce
NXP Employee
NXP Employee

Hi Oscar, 

The LCD Controller supports both Super-Twisted Nematic (STN) and Thin-Film Transistor (TFT) displays. It has a dedicated DMA controller, selectable display resolution (up to 1024 x 768 pixels), and supports up to 24-bit true-color mode.

For more information regarding the selectable display resolution you can refer to the LPC540xx/LPC54S0xx Data Sheet.

Let me know if this helps!

Sabina

1,083 次查看
oscarniño
Contributor III

Thank you so much Sabina Bruce, have a great day

0 项奖励
回复