Which is the highest resolution supported by LPC54018 MCU

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which is the highest resolution supported by LPC54018 MCU

Jump to solution
1,859 Views
oscarniño
Contributor III

Hi I want to know which is de highest resolution supported by LPC54018, right now I'm working with 480x272 resolution display touch, but I need to use a 7' display, some body could tell me?

Best regards

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,801 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hi Oscar, 

The LCD Controller supports both Super-Twisted Nematic (STN) and Thin-Film Transistor (TFT) displays. It has a dedicated DMA controller, selectable display resolution (up to 1024 x 768 pixels), and supports up to 24-bit true-color mode.

For more information regarding the selectable display resolution you can refer to the LPC540xx/LPC54S0xx Data Sheet.

Let me know if this helps!

Sabina

View solution in original post

2 Replies
1,802 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hi Oscar, 

The LCD Controller supports both Super-Twisted Nematic (STN) and Thin-Film Transistor (TFT) displays. It has a dedicated DMA controller, selectable display resolution (up to 1024 x 768 pixels), and supports up to 24-bit true-color mode.

For more information regarding the selectable display resolution you can refer to the LPC540xx/LPC54S0xx Data Sheet.

Let me know if this helps!

Sabina

1,801 Views
oscarniño
Contributor III

Thank you so much Sabina Bruce, have a great day

0 Kudos
Reply