Which is the highest resolution supported by LPC54018 MCU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Which is the highest resolution supported by LPC54018 MCU

ソリューションへジャンプ
1,891件の閲覧回数
oscarniño
Contributor III

Hi I want to know which is de highest resolution supported by LPC54018, right now I'm working with 480x272 resolution display touch, but I need to use a 7' display, some body could tell me?

Best regards

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,833件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hi Oscar, 

The LCD Controller supports both Super-Twisted Nematic (STN) and Thin-Film Transistor (TFT) displays. It has a dedicated DMA controller, selectable display resolution (up to 1024 x 768 pixels), and supports up to 24-bit true-color mode.

For more information regarding the selectable display resolution you can refer to the LPC540xx/LPC54S0xx Data Sheet.

Let me know if this helps!

Sabina

元の投稿で解決策を見る

2 返答(返信)
1,834件の閲覧回数
Sabina_Bruce
NXP Employee
NXP Employee

Hi Oscar, 

The LCD Controller supports both Super-Twisted Nematic (STN) and Thin-Film Transistor (TFT) displays. It has a dedicated DMA controller, selectable display resolution (up to 1024 x 768 pixels), and supports up to 24-bit true-color mode.

For more information regarding the selectable display resolution you can refer to the LPC540xx/LPC54S0xx Data Sheet.

Let me know if this helps!

Sabina

1,833件の閲覧回数
oscarniño
Contributor III

Thank you so much Sabina Bruce, have a great day

0 件の賞賛
返信