Using GPIO to simulate I2C?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using GPIO to simulate I2C?

2,239件の閲覧回数
lidouhe
Contributor I

Is that possible to use GPIO to simulate I2C in LPC18xx? It seem NXP don't allow the GPIO to be configured as both input and output.

ラベル(1)
0 件の賞賛
返信
1 返信

1,734件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi Lidou,

The LPC18xx contains the below features that you can use:

– One Fast-mode Plus I2C-bus interface with monitor mode and with open-drain I/O pins conforming to the full I2C-bus specification. Supports data rates of up to 1 Mbit/s.

– One standard I2C-bus interface with monitor mode and standard I/O pins.

However,  it is possible to implement a GPIO to simulate I2C, but you need to create your own algorithm and change the pin configuration between output and input every time you need.

Have a nice day!


Have a great day,

Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信