Using GPIO to simulate I2C?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using GPIO to simulate I2C?

2,182 Views
lidouhe
Contributor I

Is that possible to use GPIO to simulate I2C in LPC18xx? It seem NXP don't allow the GPIO to be configured as both input and output.

Labels (1)
0 Kudos
Reply
1 Reply

1,677 Views
soledad
NXP Employee
NXP Employee

Hi Lidou,

The LPC18xx contains the below features that you can use:

– One Fast-mode Plus I2C-bus interface with monitor mode and with open-drain I/O pins conforming to the full I2C-bus specification. Supports data rates of up to 1 Mbit/s.

– One standard I2C-bus interface with monitor mode and standard I/O pins.

However,  it is possible to implement a GPIO to simulate I2C, but you need to create your own algorithm and change the pin configuration between output and input every time you need.

Have a nice day!


Have a great day,

Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply