StartupCode LPC1517 random line issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

StartupCode LPC1517 random line issue

Jump to solution
4,024 Views
athmesh_n
Contributor IV

There is an issue in my code after removing external oscillator from custom board working on LPC1517.

IDE   :   MCUXpressoIDE

Library : REDLIB

Clock   : Internal RC Clock PLLed to 72MHz

Processor   :   LPC1517 

 

Issue:

After debug, the code jumps to some other line at start and not to main or SystemInit(). 

Error.png

Even after putting a breakpoint at cr_startup code, the issue is same.

Thanks and Regards,

Athmesh Nandakumar

 

Labels (2)
0 Kudos
Reply
1 Solution
3,870 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi ATHMESH NANDAKUMAR,

     Please check your cr_startup__lpc15xx.c file, ResetISR(void) function, this is the startup entry point after reset:

pastedImage_1.png

Enter SystemInit():

pastedImage_2.png

You can find on my side, it calls Board_systemInit();

You also need to check your code, you are calling chip_systemInit or the Board_SystemInit?

pastedImage_3.png

Do you test the official lpcopen code on your side?


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

6 Replies
3,870 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi ATHMESH NANDAKUMAR,

      What the code you are using?

     Do you use our lpc1549 lpcopen sample code on your side which just as what I recommended you?

     When you use the lpcopen code, as you know, there has two lib: chip lib and board lib.

     You need to change two lib MCU to LPC1517,

pastedImage_1.png

  Then if you want to use the internal IRC instead of the external crystal, you need to modify the board_sysinit.c function void Board_SetupClocking()

void Board_SetupClocking(void)
{
    //Chip_SetupXtalClocking();
     Chip_SetupIrcClocking();

    /* Set default system tick divder to 1 */
    Chip_Clock_SetSysTickClockDiv(1);
}

Then please build the lpc_board project again.

Now, please try it again.

Wish it helps you!
Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,870 Views
athmesh_n
Contributor IV

Capture.PNGThis is how I initialized internal clocking.

There's an issue in Internal clock interrupt. The interrupt wont work always. I am using a delay_count++ in Handler. But sometimes this delay_count wont increment. 

Debugging and putting a breakpoint in Handler does not have any effect, which means the interrupt is not working. This is my timer initialization snippet.

Thanks and Regards,

Athmesh Nandakumar

0 Kudos
Reply
3,871 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi ATHMESH NANDAKUMAR,

     Please check your cr_startup__lpc15xx.c file, ResetISR(void) function, this is the startup entry point after reset:

pastedImage_1.png

Enter SystemInit():

pastedImage_2.png

You can find on my side, it calls Board_systemInit();

You also need to check your code, you are calling chip_systemInit or the Board_SystemInit?

pastedImage_3.png

Do you test the official lpcopen code on your side?


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,870 Views
athmesh_n
Contributor IV

Thank You

0 Kudos
Reply
3,870 Views
athmesh_n
Contributor IV

The IRC has been called in main program using Chip_SetupIrcClocking();. Can it become an issue or should it be called before the _main() code in sysinit.c file?

0 Kudos
Reply
3,870 Views
athmesh_n
Contributor IV

I used the same code for changing clock setting. But sometimes the SCT interrupt wont tick. UART is now not working perfectly. 

0 Kudos
Reply