SDRAM data bytes shifting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SDRAM data bytes shifting

ソリューションへジャンプ
3,352件の閲覧回数
TEMCEFF
Contributor IV

the scenario is

when we write and read immediate it is working fine ,if we read after some time the the data bytes are shifting 2-4 bytes but occur randomly

example

the data written to SD RAM

0xA0000000 -> 0x00000000  0x44332211    0x88776655

0xA000000C->0x000000001 0x44332211    0x88776655

....

.....

data reading after some time

0xA0000000 -> 0x00000000  0x44332211    0x88778877

0xA000000C->0x000000001 0x44332211    0x88776655

 

 

the SD RAM we used is     AS4C4M16SA-6TIN

 

the timming we have initialized

are

#define SDRAM_REFRESHPERIOD_NS (64 * 1000000 / 4096) /* 4096 rows/ 64ms */
#define SDRAM_TRP_NS (21u)
#define SDRAM_TRAS_NS (42u)
#define SDRAM_TSREX_NS (67u)
#define SDRAM_TAPR_NS (20u)
#define SDRAM_TWRDELT_NS (6u)
#define SDRAM_TRC_NS (60u)
#define SDRAM_RFC_NS (60u)
#define SDRAM_XSR_NS (67u)
#define SDRAM_RRD_NS (14u)
#define SDRAM_MRD_NCLK (2u)
#define SDRAM_RAS_NCLK (2u)
#define SDRAM_MODEREG_VALUE (0x33u)
#define SDRAM_DEV_MEMORYMAP (0x05u) /* 64Mbits (4M*16, 4banks, 12 rows, 8 columns)*/

 

we used SDK emc files .

タグ(1)
0 件の賞賛
返信
1 解決策
3,224件の閲覧回数
TEMCEFF
Contributor IV

hi mike

  thanks for replay

probability is reduced when  EMC CLK is reduced to 45Mhz from 90Mhz

Refresh interval where we configure the EMC register

the information regarding Refresh interval is not provided in the datasheet.

please provided layout consideration for the SDRAM design.

if need I will send the our schematic files

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,224件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I check the Max. refresh interval time below at AS4C4M16SA datasheet:

pastedImage_2.png

pastedImage_1.png

There are some application notes about SDRAM design with LPC EMC module:

AN11508: SDRAM interface to LPC18xx/43xx EMC
− Comprehensive information about connecting EMC to different SDRAMs
− Some advanced skills like clock compensation options
− PCB layout guide

AN10771: Using the LPC24xx EMC peripheral to drive SDRAM
− Similar as AN11508, but early and simpler document

Wish it helps.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,225件の閲覧回数
TEMCEFF
Contributor IV

hi mike

  thanks for replay

probability is reduced when  EMC CLK is reduced to 45Mhz from 90Mhz

Refresh interval where we configure the EMC register

the information regarding Refresh interval is not provided in the datasheet.

please provided layout consideration for the SDRAM design.

if need I will send the our schematic files

0 件の賞賛
返信
3,224件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

First of all, thank you for the patience.

Please check below definition about SDRAM timing:

pastedImage_1.png

I checked the SDRAM timing value with below concerns:

#define SDRAM_TRP_NS (21u)      From AS4C4M16SA datasheet the value should be 18u;

#define SDRAM_TSREX_NS (67u)  is Self-Refresh Exit time, tRC+tIS = 60+1.5 , which should be 62u;

#define SDRAM_TAPR_NS (20u)   the value is 18u;

#define SDRAM_RRD_NS (14u)     should be 12u;

When you slow down the SDRAM clock frequency, if the issue happen probability reduced?


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,224件の閲覧回数
TEMCEFF
Contributor IV

hi mike

  thanks for replay

probability is not reduced when  EMC CLK is reduced to 45Mhz from 90Mhz

 

Refresh interval where we configure the EMC register

the information regarding Refresh interval is not provided in the datasheet.

please provided layout consideration for the SDRAM design.

if need I will send the our schematic files

0 件の賞賛
返信