OTP definition mismatch LPC54608

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

OTP definition mismatch LPC54608

跳至解决方案
2,089 次查看
manderson107
Contributor I

I am dealing with a mismatch between the OTP bank 3 register 0 definitions for disabling JTAG/SWD between documentation and the SDK...

SDK_2.11.1_LPC54608J512_base.tar.gz devices/LPC54608/LPC54608.h defines a JTAG disable in bit 31

UM10912 LPC546xx user manual  section 46 defines SWD_DISABLE_L and SWD_DISABLE_H on bits 3 and 10

Which one is the correct way to disable access to the device via debugger?  Obviously trial and error when blowing fuses in the OTP area is not a good approach to figuring out which one is real.  So I would appreciate a clarfication here.

 

Thanks,
Maury

 

标签 (1)
0 项奖励
回复
1 解答
2,051 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

I have reported the header file problem to SDK team. It should be fixed in SDK2.13.0.

Thanks for bringing the problem to our attention.

BR

Jun Zhang

在原帖中查看解决方案

3 回复数
2,074 次查看
manderson107
Contributor I

ok.  But my initial question still stands.  Why are these not defined in the OTPC_ECRP bit shift/mask macros in LPC54608.h

0 项奖励
回复
2,052 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

I have reported the header file problem to SDK team. It should be fixed in SDK2.13.0.

Thanks for bringing the problem to our attention.

BR

Jun Zhang

2,077 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

SWD access is decided by both FLASH ECRP and OTP ECRP

Here OTP ECRP (bit3 and bit10) is always set with higher priority than FLASH ECRP!

For detail, please see this article.
https://community.nxp.com/t5/LPC-Microcontrollers-Knowledge/LPC546xx-Understanding-ECRP/ta-p/1375263

Hope this helps.

Jun Zhang

0 项奖励
回复