LPC55S69JBD100E - SWD, JTAG and Flash programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S69JBD100E - SWD, JTAG and Flash programming

1,752件の閲覧回数
Laks489
Contributor I

1. In our project, we are using the NXP controller LPC55S69JBD100E. Is SWD and JTAG both required for programming?

2. Can you provide an explanation for the flash programming?

Laks489_1-1737701629224.pngLaks489_1-1737701629224.png

 

 

0 件の賞賛
返信
3 返答(返信)

1,582件の閲覧回数
Laks489
Contributor I

Hi , 

Does the NXP-LPC55S69JBD100 support OTA updates through bootloader when connected to the WM02C (nRF7002) via SPI? Please explain the OTA update process.

0 件の賞賛
返信

1,560件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi @Laks489 

This is a new topic regarding to OTA update. Please create a new thread for it. We will check.

 Best Regards,

Jun Zhang

0 件の賞賛
返信

1,749件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Laks489,

LPC55S69 uses SWD interface to debug and program. Jtag is for boundary scan but can't work for debug and program. 

In ISP mode, we can also use USB, UART, SPI, I2C program Flash. But we can't use these peripheral debug.

Hope this helps,

Jun Zhang

0 件の賞賛
返信