LPC55S69JBD100E - SWD, JTAG and Flash programming

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S69JBD100E - SWD, JTAG and Flash programming

1,747 Views
Laks489
Contributor I

1. In our project, we are using the NXP controller LPC55S69JBD100E. Is SWD and JTAG both required for programming?

2. Can you provide an explanation for the flash programming?

Laks489_1-1737701629224.pngLaks489_1-1737701629224.png

 

 

0 Kudos
Reply
3 Replies

1,577 Views
Laks489
Contributor I

Hi , 

Does the NXP-LPC55S69JBD100 support OTA updates through bootloader when connected to the WM02C (nRF7002) via SPI? Please explain the OTA update process.

0 Kudos
Reply

1,555 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi @Laks489 

This is a new topic regarding to OTA update. Please create a new thread for it. We will check.

 Best Regards,

Jun Zhang

0 Kudos
Reply

1,744 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Laks489,

LPC55S69 uses SWD interface to debug and program. Jtag is for boundary scan but can't work for debug and program. 

In ISP mode, we can also use USB, UART, SPI, I2C program Flash. But we can't use these peripheral debug.

Hope this helps,

Jun Zhang

0 Kudos
Reply