LPC55S36 ETM Trace with IAR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S36 ETM Trace with IAR

1,662 Views
jpholme
Contributor II

How does one utilize ETM trace debugging on the LPC55S36?

I have activated the 5 pins P1_1, P0_24, P0_28, P0_29 and P0_30 with mode 5 and 6 resp. to activate the outputs.

I have experimented with Debugger, I-JET settings under Trace, but nothing really seems to activate the icon during debugging.

What am I missing?

0 Kudos
Reply
1 Reply

1,641 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

First of all, the LPC553x have ETM module and support trace function.

But the trace function requires dedicated hardware device and software tools, pls refer to the an14330.pdf, which I attached. Although it focuses on the i.mxrt, it also adapts to LPC family.

Hope it can help you

BR

XiangJun Rong

 

0 Kudos
Reply