LPC55S36 ETM Trace with IAR

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC55S36 ETM Trace with IAR

2,442 次查看
jpholme
Contributor II

How does one utilize ETM trace debugging on the LPC55S36?

I have activated the 5 pins P1_1, P0_24, P0_28, P0_29 and P0_30 with mode 5 and 6 resp. to activate the outputs.

I have experimented with Debugger, I-JET settings under Trace, but nothing really seems to activate the icon during debugging.

What am I missing?

0 项奖励
回复
1 回复

2,421 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

First of all, the LPC553x have ETM module and support trace function.

But the trace function requires dedicated hardware device and software tools, pls refer to the an14330.pdf, which I attached. Although it focuses on the i.mxrt, it also adapts to LPC family.

Hope it can help you

BR

XiangJun Rong

 

0 项奖励
回复