LPC55S36 ETM Trace with IAR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S36 ETM Trace with IAR

2,451件の閲覧回数
jpholme
Contributor II

How does one utilize ETM trace debugging on the LPC55S36?

I have activated the 5 pins P1_1, P0_24, P0_28, P0_29 and P0_30 with mode 5 and 6 resp. to activate the outputs.

I have experimented with Debugger, I-JET settings under Trace, but nothing really seems to activate the icon during debugging.

What am I missing?

0 件の賞賛
返信
1 返信

2,430件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

First of all, the LPC553x have ETM module and support trace function.

But the trace function requires dedicated hardware device and software tools, pls refer to the an14330.pdf, which I attached. Although it focuses on the i.mxrt, it also adapts to LPC family.

Hope it can help you

BR

XiangJun Rong

 

0 件の賞賛
返信