LPC1833 external SPI flash bootloader

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1833 external SPI flash bootloader

2,462 次查看
tony567
Contributor III

Hi, there,

   I am not sure if this community is alive or not, but I have no other way to solve my issue which stucks me more than 2 months cause I am totally a hardware designer, know little about coding, but no one can help me for this.

here my issue is we implement 2 second source external SPI flash IC for LPC1833, so the original bootloader for one time FW updating into flash is nolonger workable for new SPI flash ICs, the situation now is the original bootloader source code has lost, and no one know the next step in my company

now I need help from NXP,

1. does NXP have example code for LPC1833 external SPI Flash bootloader?

2. could NXP support to teach us how to modify the bootloader code for new SPI flash?

3. if NXP don't support to teach how to modify the bootloader code, is there any reference documents for LPC1833 external SPI flash bootloader?

4. could NXP support to teach the steps to set the MCUXpresso IDE v11.3.1_5262 and Keil uVision5 for LPC1833 external SPI flash bootloader code compile?

 

标签 (3)
0 项奖励
回复
2 回复数

2,453 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello  tony567,

There is a SPI second bootloader for LPC17xx, you can refer to:

https://www.nxp.com/docs/en/application-note/AN11257.zip  

 

BR

Alice

0 项奖励
回复

2,444 次查看
tony567
Contributor III

Hi, Alice,

   thanks your reply, but this file is for master MCU and slave MCU...

0 项奖励
回复