LPC1833 external SPI flash bootloader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1833 external SPI flash bootloader

2,463件の閲覧回数
tony567
Contributor III

Hi, there,

   I am not sure if this community is alive or not, but I have no other way to solve my issue which stucks me more than 2 months cause I am totally a hardware designer, know little about coding, but no one can help me for this.

here my issue is we implement 2 second source external SPI flash IC for LPC1833, so the original bootloader for one time FW updating into flash is nolonger workable for new SPI flash ICs, the situation now is the original bootloader source code has lost, and no one know the next step in my company

now I need help from NXP,

1. does NXP have example code for LPC1833 external SPI Flash bootloader?

2. could NXP support to teach us how to modify the bootloader code for new SPI flash?

3. if NXP don't support to teach how to modify the bootloader code, is there any reference documents for LPC1833 external SPI flash bootloader?

4. could NXP support to teach the steps to set the MCUXpresso IDE v11.3.1_5262 and Keil uVision5 for LPC1833 external SPI flash bootloader code compile?

 

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

2,454件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello  tony567,

There is a SPI second bootloader for LPC17xx, you can refer to:

https://www.nxp.com/docs/en/application-note/AN11257.zip  

 

BR

Alice

0 件の賞賛
返信

2,445件の閲覧回数
tony567
Contributor III

Hi, Alice,

   thanks your reply, but this file is for master MCU and slave MCU...

0 件の賞賛
返信