KEIL with LPC1549 Xpresso V2 : no Cortex-M SW device found

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KEIL with LPC1549 Xpresso V2 : no Cortex-M SW device found

6,304件の閲覧回数
rajeshsh_
Contributor I

Dear All,

I am using LPC1549 Xpresso V2 board and flashed "Firmware_JLink_LPCXpresso_V20160530.bin" J-Link debug probe firmware using LPCScript command line utility.

To flash application from KEIL uVision5, I selected Debug option as : J-Link/J-TRACE Cortex, and under settings, I see the following :

under Device Name: no SW-DP found

After that, when try to download the application, the KEIL shows : no Cortex-M SW device found.

Can anyone please suggest how to fix this issue?

Also, Can anyone please let me know where can I get CMSIS-DAP image for debug probe for LPC15xx series?

Please find attached 3 images attached for Your reference.

 

Regards,

Raj. S

ラベル(3)
タグ(2)
0 件の賞賛
返信
1 返信

5,371件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

The latest CMSIS-DAP image for LPCXpresso V2 and V3 boards, such as the LPCXpresso1549 is also provided as part of the LPCScrypt deliverables.

Information on the latest LPCScrypt release can be found at: LPCScrypt - Latest Release : v1.8.0

And more information includes downloads can be found at:  https://www.nxp.com/pages/:LPCSCRYPT​​

General information on programming up the debug firmware can be found at:

LPC-Link2 Debug Probe firmware programming

And Segger's notes on using the LPCXpresso boards with their firmware can be found at:

https://www.segger.com/jlink-lpcxpresso-ob.html

I can't help you with using Keil tools or the Segger J-Link image, but I would suggest the first thing to do is confirm how your board enumerates inside Windows after you plug it in (in "Devices and Printers").

Regards,

LPCXpresso Support

0 件の賞賛
返信