LPCScrypt - Latest Release : v1.8.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCScrypt - Latest Release : v1.8.2

LPCScrypt - Latest Release : v1.8.2

To download installers for all platforms, please visit:

http://www.nxp.com/pages/:LPCSCRYPT

 

Latest release: v1.8.2 (build 753), 19 June 2017

  • Added support for new SPIFI devices:
    • GD25Q32C, MT25QL128AB, MX25R6435F
  • Updated binary for CMSIS-DAP debug probe firmware with new features (to ..V5_182).
  • Updated binary for Segger J-Link debug probe firmware (to .._20160923).
  • Added code to deal with Winbond status CMP bit erroneously becoming set so preventing programming
  • Added note that references to LPCXpresso IDE now equally apply to the new MCUXpresso IDE
  • Various minor additions, bug and documentation fixes

Previous release: v1.8.0 (build 723), 20 July 2016

  • Added support for new SPIFI devices:
    • N25Q32, N25Q64, N25Q256, MT25QL256A, MT25QL512A, MX25V8035F, MX25L12835E
  • Updated binary for CMSIS-DAP debug probe firmware with new features (to ..V5_173):
  • Updated binary for Segger J-Link debug probe firmware (to ..V20160530).
  • Improved reliability of CMSIS-DAP and J-Link firmware programming scripts
  • Improved LPCScrypt_CLI on Mac/Linux to support ReadLine history
  • Fixed host crash on Mac when large quantity of data is printed
  • Various minor additions, plus bug and documentation fixes

 

v1.7.1 (internal)

  • Added beta support for new SPIFI device - Micron N25Q256, please note:
    • Chip Erase and Programming (with automatic inline verify) expected to work without issue
    • BootROM booting with this part is only supported in BootROM versions 11.2 and 12.2, this functionality has not been tested during LPCScrypt development
  • Improved BootROM version reporting
  • Added simple LPCScrypt_CLI scripts to provide pseudo command line experience with automatic firmware booting
  • Fixed issue with temp files on Linux hosts
  • Various minor bug and documentation fixes

 

Previous release: v1.7 build 696, 23 Feb 2016

  • Added flashSet command (as a superset and replacement of EEPROMset) to enable patching of word in all supported flash memories
    • usage -  flashSet flash+offset value
  • CMSIS-DAP programming script displays probe serial number/ID
  • Updated binary for CMSIS-DAP debug probe firmware incorporating new features (to ..V5_147):
    • support for power measurement averaging with specific LPCXpresso V3 boards
    • probe enumeration as a unique device by adding an ascii representation of the debug probe MCU's serial number
      • enabling multiple LPC-Link2 debug probes to be used and identified in single of multiple debug sessions within the LPCXpressoIDE v8.1
  • Various minor bug fixes

 

Previous release : v1.6 build 652, 26 Nov 2015

  • Added automatic verify of all flash programming operations
  • Added commands for various SPIFI operations
  • Updated binary for CMSIS-DAP debug probe firmware with new features (to ..V5_134)
  • Updated binary for Segger J-Link debug probe firmware (to ..V20151006)
  • Added support for new SPIFI device - N25Q128

 

Previous release : v1.5.2 build 588, 23 June 2015

  • Windows Only: Added Start menu shortcuts for booting LPCScrypt and programming debug probe firmware
  • Windows Only: Added CMSIS-DAP driver to drivers directory
  • Improved scripts to program debug probe firmware

 

Previous release : v1.5 build 562, 1 June 2015

  • Added binaries for CMSIS-DAP (V5.112) and Segger J-Link debug probe firmware
  • Added scripts to enable easy programming of CMSIS-DAP and J-Link firmware
  • Added Debug Probe Firmware Programming guide
  • Added support for new SPIFI devices – W25Q128FV and MX25L1606

 

Previous release : v1.3 build 496, 12 March 2015

  • Added support for connections via USB1 as well as USB0
  • Added support for new SPIFI devices – W25Q40CV and PM25LQ032C

 

Currently supported SPIFI devices:

  • GD25Q32C
  • MT25QL128AB
  • MT25Q512A
  • MT25Q256A
  • N25Q256
  • N25Q128
  • N25Q64
  • N25Q32
  • PM25LQ032C
  • MX25L1606E
  • MX25L1635E
  • MX25L3235E
  • MX25R6435F
  • MX25L6435E
  • MX25L12835E
  • MX25V8035F
  • MX25L8035E
  • S25FL016K
  • S25FL032P
  • S25FL064P
  • S25FL129P 64kSec
  • S25FL129P 256kSec
  • S25FL164K
  • S25FL256S 64kSec
  • S25FL256S 256kSec
  • S25FL512S
  • W25Q40CV
  • W25Q32FV
  • W25Q64FV
  • W25Q128FV
  • W25Q256FV_Untested
  • W25Q80BV
No ratings
Version history
Last update:
‎07-19-2016 07:36 AM
Updated by: