Can LPC4078 GPIO invert before UART receive?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can LPC4078 GPIO invert before UART receive?

ソリューションへジャンプ
1,559件の閲覧回数
matthewryan
Contributor I

I want to invert an incoming signal before entering my UART on the LPC4078.  Can anyone confirm that the LPC4078, thru use of the D_IOCON register, bit 6 "INV", can invert this signal before it enters the UART RX peripheral?  I've done this on the LPC812 before, but have not used the LPC4078 before...

Thanks!

ラベル(1)
0 件の賞賛
返信
1 解決策
1,415件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Matthew Ryan,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.

The 'INV' feature is available when pin selects UART RX function, and you can give it a try

Ping

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

元の投稿で解決策を見る

2 返答(返信)
1,416件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Matthew Ryan,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.

The 'INV' feature is available when pin selects UART RX function, and you can give it a try

Ping

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

1,415件の閲覧回数
matthewryan
Contributor I

Thank you...

0 件の賞賛
返信