Can LPC4078 GPIO invert before UART receive?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can LPC4078 GPIO invert before UART receive?

Jump to solution
2,337 Views
matthewryan
Contributor I

I want to invert an incoming signal before entering my UART on the LPC4078.  Can anyone confirm that the LPC4078, thru use of the D_IOCON register, bit 6 "INV", can invert this signal before it enters the UART RX peripheral?  I've done this on the LPC812 before, but have not used the LPC4078 before...

Thanks!

Labels (1)
0 Kudos
Reply
1 Solution
2,193 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Matthew Ryan,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.

The 'INV' feature is available when pin selects UART RX function, and you can give it a try

Ping

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

View solution in original post

2 Replies
2,194 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Matthew Ryan,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.

The 'INV' feature is available when pin selects UART RX function, and you can give it a try

Ping

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

2,193 Views
matthewryan
Contributor I

Thank you...

0 Kudos
Reply