Bricked PN5190 via Secure Upgrade via NXP NFC Cockpit

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Bricked PN5190 via Secure Upgrade via NXP NFC Cockpit

跳至解决方案
5,021 次查看
Avis
Contributor II

Hello,

I have NXP S32K144EVB-Q100 board and NXP NCx3321 S32K Addon Board3.Before the software was Firmware_2.05.

The problem I have is that when updating Secure Upgrade to PN5190Firmware_2.F7.esfwu, updated failed.

The board doesnt work anymore.
Log Monitor:
2024.04.05 13:00:05]:INFO:BoardDetect:Enforcing board selection for PN5190
2024.04.05 13:00:05]:INFO:ServiceFactory:Generating Services for VCOM_PN5190 @COM57
2024.04.05 13:00:06]:ERROR:App:Internal Error occurred "The operation has timed out." in System
2024.04.05 13:00:07]:ERROR:App:Internal Error occurred "The operation has timed out." in System
2024.04.05 13:00:08]:ERROR:App:Internal Error occurred "The operation has timed out." in System
2024.04.05 13:00:09]:ERROR:App:Internal Error occurred "The operation has timed out." in System
2024.04.05 13:00:11]:ERROR:App:Internal Error occurred "The operation has timed out." in System
2024.04.05 13:00:11]:ERROR:ABalDelegate:Error while querying PIN_IRQ. GENERIC,USE_CONDITION
2024.04.05 13:00:11]:WARN:ABalDelegate:Waited for PIN_IRQ to go High. Timed out.
2024.04.05 13:00:12]:ERROR:App:Internal Error occurred "The operation has timed out." in System
2024.04.05 13:00:12]:ERROR:ServiceFactory:InitHALPN5190.ApplyProtocolSettings failed. Status=240,IO_TIMEOUT
2024.04.05 13:00:12]:ERROR:ServiceFactory:InitHALPN5190() failed. Status=240,IO_TIMEOUT
2024.04.05 13:00:12]:ERROR:ServiceFactory:Previous FW Download to PN5190 seems to be incomplete. You may have to perform Secure FW Upgrade again
2024.04.05 13:00:12]:INFO:SecureFWUpgrade:Entering download mode
2024.04.05 13:00:13]:ERROR:App:Internal Error occurred "The operation has timed out." in System
2024.04.05 13:00:14]:ERROR:App:Internal Error occurred "The operation has timed out." in System
2024.04.05 13:00:15]:ERROR:App:Internal Error occurred "The operation has timed out." in System
2024.04.05 13:00:16]:INFO:SecureFWUpgrade:Entered download mode
2024.04.05 13:00:17]:ERROR:App:Internal Error occurred "The operation has timed out." in System
2024.04.05 13:00:18]:ERROR:App:Internal Error occurred "The operation has timed out." in System
2024.04.05 13:00:19]:ERROR:App:Internal Error occurred "The operation has timed out." in System
2024.04.05 13:00:19]:ERROR:ABalDelegate:Error while querying PIN_BUSY. GENERIC,USE_CONDITION
2024.04.05 13:00:19]:INFO:SecureFWUpgrade:Resetting Reader IC (FrontEnd) to enter normal mode
2024.04.05 13:00:20]:ERROR:App:Internal Error occurred "The operation has timed out." in System
2024.04.05 13:00:21]:ERROR:App:Internal Error occurred "The operation has timed out." in System
2024.04.05 13:00:22]:ERROR:App:Internal Error occurred "The operation has timed out." in System
2024.04.05 13:00:22]:INFO:SecureFWUpgrade:Reader IC (FrontEnd) Reset complete.
2024.04.05 13:00:24]:ERROR:App:Internal Error occurred "The operation has timed out." in System
2024.04.05 13:00:25]:ERROR:App:Internal Error occurred "The operation has timed out." in System
2024.04.05 13:00:26]:ERROR:App:Internal Error occurred "The operation has timed out." in System
2024.04.05 13:00:27]:ERROR:App:Internal Error occurred "The operation has timed out." in System
2024.04.05 13:00:28]:ERROR:App:Internal Error occurred "The operation has timed out." in System
2024.04.05 13:00:29]:ERROR:App:Internal Error occurred "The operation has timed out." in System
2024.04.05 13:00:30]:ERROR:App:Internal Error occurred "The operation has timed out." in System
2024.04.05 13:00:31]:ERROR:App:Internal Error occurred "The operation has timed out." in System
2024.04.05 13:00:31]:INFO:ServiceFactory:Retrieved FW version from Secure Download Mode: 0.0
2024.04.05 13:00:31]:ERROR:ServiceFactory:GenerateServices (VCOM_PN5190 @COM57) Failed with 240,IO_TIMEOUT
2024.04.05 13:00:32]:ERROR:App:Internal Error occurred "The operation has timed out." in System
2024.04.05 13:00:33]:ERROR:App:Internal Error occurred "The operation has timed out." in System
2024.04.05 13:00:33]:INFO:ServiceFactory:uC FW Version: (Compiled on )
2024.04.05 13:00:34]:ERROR:App:Internal Error occurred "The operation has timed out." in System
2024.04.05 13:00:35]:ERROR:App:Internal Error occurred "The operation has timed out." in System
2024.04.05 13:00:36]:ERROR:App:Internal Error occurred "The operation has timed out." in System
2024.04.05 13:00:37]:ERROR:App:Internal Error occurred "The operation has timed out." in System
2024.04.05 13:00:38]:ERROR:App:Internal Error occurred "The operation has timed out." in System
2024.04.05 13:00:39]:ERROR:App:Internal Error occurred "The operation has timed out." in System
2024.04.05 13:00:39]:ERROR:ServiceFactory:Bal, Hal, OSal Initialization (VCOM_PN5190 @COM57) Failed with 240,IO_TIMEOUT

port.png

Thank you for taking the time to repair the board.

Regards
Avis

0 项奖励
回复
1 解答
4,640 次查看
Avis
Contributor II
Hello, the problem is Fixed.
BR
Avis

在原帖中查看解决方案

0 项奖励
回复
5 回复数
4,641 次查看
Avis
Contributor II
Hello, the problem is Fixed.
BR
Avis
0 项奖励
回复
4,665 次查看
Avis
Contributor II

Hello, @KaiLi
The EEPROM from the antena NFC is clear.
To solve this issue need be chip soldered.

NXP S32K144EVB-Q100 is working correct.
BR
Avis

0 项奖励
回复
3,491 次查看
zhouwenlu
Contributor I

I am having the same problem as you, can I ask how to solder the chip. Can you share any specific instructions?

0 项奖励
回复
4,681 次查看
KaiLi
NXP TechSupport
NXP TechSupport

Hello @Avis 

It's recommended that you log in https://www.docstore.nxp.com/

to download UM789513 and refer it to configurate your device.

KellyLi_0-1712568600400.png

BR

Kelly

0 项奖励
回复
2,107 次查看
ctfy
Contributor I
my 5180 have same probrem ,and i can‘t download um789513 .do you have any other advice
0 项奖励
回复