Kinetis Software Development Kit Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis Software Development Kit Knowledge Base

Labels

Discussions

Sort by:
Hello Kinetis users!   I thought this would be the best place to share this code.  Attached is an example of how to use the power manager in the 1.0.0 release of the Kinetis SDK.  It is essentially the legacy low power demo ported to the SDK.  Now, the SDK doesn't provide functions to de-initialize the pins so some of it is a little messy, but it should still help to show you how to use the power manager and how to get in and out of low power modes.    The supported platforms are:   FRDM-K22F FRDM-K64F TWR-K22F120M TWR-K64F120M TWR-KV31F120M   To install the demo, simply unzip the file to the "demos" folder of your SDK installation.  All of the links in the demo are relative so you shouldn't have any trouble.  However, if you do experience any issues, please let me know so that I can correct the issues.    To run the demo, simply build and download the application (a guide of how to do this is provided in the device specific User's Guide in your SDK installation).  Then perform a power-on reset (you always want to do that when working with low power applications) and connect a terminal utility with the following settings:   - 19200 baud rate - 8 data bits - No parity - 1 stop bit - No flow control   Then follow the on-screen instructions.    As a reminder to those wishing to understand low power operations and the Kinetis devices a little more, we do have an Application Note out there to help explain low power operations:  AN4503 Power Management for Kinetis and ColdFire+ MCUs.  This Application Note is in the process of being updated with Kinetis SDK information and is scheduled to be re-published sometime this year.    Enjoy! Chris
View full article
For installation standalone KSDK packages please follow these instructions:   Go to www.freescale.com/ksdk and click to download Is needed to be signed in After that is seen standalone package for FRDM-KL43Z and KL33Z Agree with Software Terms and Conditions Choose installation package according to platform Save file and install it After installation, final folder appears at C:\Freescale\KSDK1.2.0_KL33Z_1.0.0 and Eclipse update - import package to KDS from C:\Freescale\KSDK1.2.0_KL33Z_1.0.0\tools\eclipse_update   Eclipse Update In KDS choose Install New Software Click Add Choose Archive Choose the Eclipse Update zip file located at C:\Freescale\KSDK1.2.0_KL33Z_1.0.0\tools\eclipse_update Select update for KL33Z and KL43Z Accept terms of the license agreement   🙂 Enjoy!
View full article
The one way how to set TAD shell is to use current example shell for e.g. FRDM-K64F, modified it and use it.   1. Open demo Shell (located at C:\Freescale\KSDK_1.2.0\middleware\tcpip\rtcs\examples\shell\build\kds\shell_frdmk64f) in KDS, as .wsd file 2. Open demo_cmd.c (located at /shell_frdmk64f/Source/demo_cmd.c) and add the line for shell tad, { "echosrv",   Shell_echosrv},     { "echo",      Shell_echo},     { "email",     Shell_smtp },     { "gate",      Shell_gate },     { "gethbn",    Shell_get_host_by_name },     { "getname",   Shell_getname },     { "getrt",     Shell_getroute },     { "ipconfig",  Shell_ipconfig },     { "llmnr",  Shell_llmnrsrv }, { "tad",  Shell_tad },   3. Open tad.c (located at /mqx_frdmk64f/MQX_Generic/tad/tad.c) and remove at the first line:         #if MQX_USE_IO_OLD and last line        #endif // MQX_USE_IO_OLD and included fio library       #include <fio.h>    4. Build libraries first, then build demo shell_frdmk64 5. Set the Tera Term and after typing tad in Tera Term, you will see the output:   Enjoy!   Iva
View full article
Because I receive feedback from customers, that it is sometimes complicated to execute this demo, I created short tutorial how to set it and execute it in KDS 3.0.0.   1. Physical connection In case of TWR-K64F, is needed TWR-SER and correctly set jumpers. and for TWR-K64F is needed to set jumper J6 to pins 1 and 2.   Be sure, that the TWR-SER and TWR-K64F is correctly connected (by white line) 2. Network configuration For changing IP address, please go to Network and Sharing Center, choose Change adapter settings Right click on Properties and change the IP address (TCP/IPv4) to 192.168.2.100   3.  Downloading the demo to TWR-K64F Go to KDS, File - Import and browse the demo, which is located at C:\Freescale\KSDK_1.2.0\examples\twrk64f120m\demo_apps\web_hvac\web_hvac_mqx\kds Import all libraries and the demo project and see imported sets in Project Explorer Debug the libraries first and then the project. Be sure, what debugger is used on the board and set the debugger. And now go to Resume!   4. Test the connection Go to cmd and ping to 192.168.2.102 (address of HVAC Server)   5. HVAC Web Server.Go to browser and type the address 192.168.2.102, you will see page for HVAC Web Server. Go to HVAC Demo - HVAC Status and now you can observe the temperatures by pressing button. There are set combinations which means see below. LED1: Simulate the Fan’s state LED2: System in the Heat mode LED3: System in the Cool mode LED4: Simulate the heart beat, increase real temperature (i.e., by hair dryer) to see the LED4 go faster and decrease temperature to see it slow down. So, if is needed increased temperature, push the first button (SW1) and Fan and Heat mode run. LED1 and LED2 will be light on and the temperature will increase.   Enjoy! Iva
View full article
Recently one of our customers reported an issue when he tried to run "dspi_edma_demo" with KSDK 1.0 on K22F freedom board. He connected SPI signals between master and slave according to the demo user guide on freedom board, but the demo was not working.   I reproduced the issue on freedom and found this is due to incorrect documentation in demo user guide.   The connection table shown in demo user guide for K22F freedom board is as follows. This is not correct.   It should be the following table instead.  Master Connects to Slave Signal Pin Name Board Location Pin Name Board Location SS PTD0 J6 Pin 8 -> PTD4 J2 Pin 6 SCK PTD1 J6 Pin 5 -> PTD5 J2 Pin 12 Data Out PTD2 J6 Pin 6 -> PTD7 J2 Pin 10 Data In PTD3 J6 Pin7 -> PTD6 J2 Pin 8   Also, the associated pin mux configuration in pin_mux.c file should be changed from the original workaround one in red to the original commented one.   void pin_mux_SPI(uint32_t instance)   {     switch(instance) {       case 0:                             /* SPI0 */         /* PORTD_PCR0 */         PORT_HAL_SetMuxMode(g_portBaseAddr[3],0u,kPortMuxAlt2);         //PORT_HAL_SetMuxMode(g_portBaseAddr[2],4u,kPortMuxAlt2);   /*** Temporary work around until next board spin. ***/         /* PORTD_PCR3 */         PORT_HAL_SetMuxMode(g_portBaseAddr[3],3u,kPortMuxAlt2);         //PORT_HAL_SetMuxMode(g_portBaseAddr[2],5u,kPortMuxAlt2);   /*** Temporary work around until next board spin. ***/         /* PORTD_PCR1 */         PORT_HAL_SetMuxMode(g_portBaseAddr[3],1u,kPortMuxAlt2);         //PORT_HAL_SetMuxMode(g_portBaseAddr[2],6u,kPortMuxAlt2);   /*** Temporary work around until next board spin. ***/         /* PORTD_PCR2 */         PORT_HAL_SetMuxMode(g_portBaseAddr[3],2u,kPortMuxAlt2);         //PORT_HAL_SetMuxMode(g_portBaseAddr[2],7u,kPortMuxAlt2);   /*** Temporary work around until next board spin. ***/         break;   }   }  
View full article
Kinetis SDK v2 is here! Introducing Kinetis SDK v2 The first steps with KSDK How to start with KSDK* List of published examples: KSDK list of examples* List of published documents: KSDK list of documents* * All of the source code placed in spaces above is for example use only. NXP does not accept liability for use of this code in the user’s application.
View full article