No .wsd file generated by KSDK Project Generator for FRDMK82F board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No .wsd file generated by KSDK Project Generator for FRDMK82F board

2,555 Views
shivamgautam
Contributor I

I was trying to generate project for my frdmk82f board using the KSDK Project Generator (Basic). I've selected the SDK location, Selected my board and then clicked Generate. It Generates the folder but under kds folder there is no myProject.wsd file generated which I can import to Kinetis Design Studio. Please Help.

Labels (1)
4 Replies

2,227 Views
enriqueolivieri
Contributor I

I have the same problem. I use KSDK Project Generator 2.2 and doesn't generate the .wsd

0 Kudos
Reply

2,227 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi,
Actually .wsd file is not needed to import KDS project.

Just use File - Import - General - Existing Project into Workspace and select "kds" directory inside new project directory structure.


".wsd" file was useful for SDK 1.3, where several projects was needed to import (e.g. library project and example project). For SDK 2.x library project is not needed anymore.

Hope this helps

Jorge Alcala

2,227 Views
enriqueolivieri
Contributor I

jorge_a_vazquez escribió:

Hi,
Actually .wsd file is not needed to import KDS project.

 

Just use File - Import - General - Existing Project into Workspace and select "kds" directory inside new project directory structure.


".wsd" file was useful for SDK 1.3, where several projects was needed to import (e.g. library project and example project). For SDK 2.x library project is not needed anymore.

 

Hope this helps

Jorge Alcala

Thank You for your help

0 Kudos
Reply

2,227 Views
ivadorazinova
NXP Employee
NXP Employee

Hello Shivam,

yes, you are absolutely right.

I can confirm the same behavior on my side.

For KDS the .wsd file was not generated.

Thank you for pointing out this bug!

I already reported to Project Generator team. PGKSDK-343

I will keep you informed.

Best Regards,

Iva

0 Kudos
Reply