Documentation for current KSDK 1.3 is located under C:\Freescale\KSDK_1.3.0\doc
Application Notes and another documents are located under Software Development Kit for Kinetis MCUs|NXP
There are more documents, which were created:
KSDK 2.0
Using Kinetis Design Studio v3.x with Kinetis SDK v2.0
KSDK 1.3
How to add SD card support in the composite msd_cdc demo[KSDK 1.3]
KSDK Clock configurations and Low Power modes with Processor Expert
New Kinetis SDK Project Generator v2 is available!
KSDK Project Generator - BUG workaround
KSDK 1.3 Documents Plugin in KDS - is available now!
KSDK 1.3.0 Documents Plugin for KDS 3.0.0
KSDK 1.2
Interrupt handling with KSDK and Kinetis Design Studio
Creating a New USB project with KSDK and Processor Expert support in KDS
IAR MQX TAD solution for "Unknown error" in Task error code (with KSDK)
How to Add lwIP to KDS3.0 Project
How to: Create a New FreeRTOS for KSDK1.2 Project in KDS3.0
How to Create a C++ Project Using MQX RTOS for KSDK1.2
How to implement a USB Device MSD demo based on KSDK PEx components and KDS 3.0
How to: execute the demo HVAC on lwIP TCP/IP Stack in KSDK
Adding TAD shell in KSDK shell demo
FRDM-KL43Z and KL33Z - standalone package
Getting started with KSDK: Building the demo applications
KSDK 1.1
How to create copy of KSDK example in KDS
KSDK 1.0