UART Example with KSDK

Document created by Iva Susnova Employee on Apr 6, 2015Last modified by ebiz_ws_prod on Dec 13, 2017
Version 4Show Document
  • View in full screen mode

I created easy tutorial for UART KSDK blocking demo which works as echo.

The demo works with KSDK 1.1. and is created for KDS 2.0.

 

Because it could be problem if was used this pin

by this reason was chosen UART 3, which is available to use and is routed to PTC16,PTC17

connection on Arduino header

for this case is use ALT3 function (PTC16, PTC17)

 

Final output from terminal

Physical connection between FRDM-K64F and USB to Serial Converter

IMG_0532.JPG

The unzipped folder must be located in example folder at C:\Freescale\KSDK_1.1.0\demos\

Original Attachment has been moved to: uart_blocking_frdmk64f.zip

Attachments

    Outcomes