Controlling a pin with GPIO and Output compare

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Controlling a pin with GPIO and Output compare

2,307 Views
therealfreegeek
Contributor IV

Board - FRDMK64

KSDK - 1.3

KDS - 3 with all the updates

 

I tried to set up the GPIO driver for PTD0 and the FTM output compare driver for  FTM3 Ch0 on PTD0 but PE says there is a conflict and will not allow it.

 

It this expected behaviour?

 

Cheers

Jim

Labels (1)
0 Kudos
Reply
3 Replies

2,143 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Ernest,

Does your project is about KSDK ?

If yes, you can refer to the  attached method to share PTD0 pin.

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,143 Views
therealfreegeek
Contributor IV

Hi Alice, yes KDSK 1.3, I will try your suggestion.

Thanks

Jim

0 Kudos
Reply

2,143 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Jim,

Ok, hope it helps , waiting your result , if have any question about it , please contact

me without any hesitate.

BR

Alice

0 Kudos
Reply