BOARD_BootClockRUN for MK22FN128VLH10

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BOARD_BootClockRUN for MK22FN128VLH10

4,017件の閲覧回数
양승도
Contributor II

I faced a trouble with the configuration of the BOARD_BootClockRUN for MK22FN128VLH10.

I want to configure MCG mode FEE, FLL output 80MHz, Core clock 80MHz, Bus clock 40MHz, Flash clock 20MHz.

IDE: KDS 3.2

SDK: 2.1

MCU: MK22FN128VLH10

 

How to configure BOARD_BootClockRUN for 80MHz in MK22FN128VLH10?

 

Best Regards,

Frank Yang

ラベル(1)
0 件の賞賛
返信
7 返答(返信)

3,705件の閲覧回数
양승도
Contributor II

There is no hardware problem for Oscillator (OSC).

This target board is good to operate with KSDK 1.3.

I think your SDK has a problem.

Clock operation is not good with SKD 2.1 in the same hardware condition.

but Clock operation is good with KSDK 1.2, KSDK 1.3 and ProcessorExpert in the same hardware condition.

and this hardware has been used for 1 year and half. and there is no problem yet at the point of clock operation.

0 件の賞賛
返信

3,705件の閲覧回数
양승도
Contributor II

Clock is generated but it is not sine wave and wrong operation example code.

It is waveform from EXTAL0 pin.

unstable clock.png

ther broken chracteristics of the uart interrupt example in SDK 2.1.

broken characters.png

Attached is the generated clock configuration tool file:

MK22FN128xxx10_clocks_sources_2017-02-15_00_44

0 件の賞賛
返信

3,705件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hello Frank,

It seems to be an issue of the oscillator circuit design. Please, verify the design according to reference manual of the MK22FN128xxx10 - Oscillator (OSC) chapter and datasheet of the crystal oscillator. You must use the correct crystal oscillator connection and components. You can also find additional details in the Crystal Oscillator Troubleshooting Guide (see http://www.nxp.com/assets/documents/data/en/application-notes/AN3208.pdf).

Best Regards,

Marek Neuzil

0 件の賞賛
返信

3,705件の閲覧回数
양승도
Contributor II

I generated the code from Clock Tool in your web site.

Even thought generating the code and X-tal hardware was verified with processorExpert in the past, it didn't work.

Now, it works after marking // some lines: wait and check status as following: I think it is not normal.

status_t CLOCK_SetFeeMode(...)

{

...

/* Wait and check status. */

//while(kMCG_FllSrcExternal != MCG_S_IREFST_VAL)

//{

//}

...

}

marked the wait and check status.png

Clock Frequency is nothing at probe to x-tal hardware, EXTAL0, XTAL0.

I attached the files which was generated in you web site.

MK22FN128xxx10_clocks_sources_2017-02-13_10_28

MK22FN128xxx10_pins_sources_2017-02-13_03_26

0 件の賞賛
返信

3,705件の閲覧回数
양승도
Contributor II

After choosing OSC mode : Using oscillator with external crystal (low power)

CLOCK_SetExternalRefClkConfig.png

0 件の賞賛
返信

3,705件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hello Frank,
I have analyzed you source code and you have selected incorrect configuration of the OSC. When you connect external crystal you must select an external crystal mode and frequency range (and capacity if required). In your application the external reference clock is selected (EXTAL0 pin only is used).

See the following screenshot for details:

 pastedImage_2.png

Note:

SDK 2.0 contains a defect - when FEE mode is selected and OSCERCLK is disabled the initialization code does not finished (a while loop does not finish due to an error). Enable OSCERCLK as a workaround for this issue.

Best Regards,

Marek Neuzil

0 件の賞賛
返信

3,705件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Frank,

i think you can use the code to set the MCG in FEE mode, but you have to connect the crystal to Extal/Xtal or Extal32/Xtal32 pins and know the clock frequency of crystal, so that you can figure out frdiv, drs parameters.

void BOARD_BootClockRUN(void)
{
    CLOCK_SetSimSafeDivs();

    CLOCK_InitOsc0(&g_defaultClockConfigRun.oscConfig);
    CLOCK_SetXtal0Freq(BOARD_XTAL0_CLK_HZ);

   /* CLOCK_BootToPeeMode(g_defaultClockConfigRun.mcgConfig.oscsel, kMCG_PllClkSelPll0,
                        &g_defaultClockConfigRun.mcgConfig.pll0Config);*/

CLOCK_BootToFeeMode(
    mcg_oscsel_t oscsel, uint8_t frdiv, mcg_dmx32_t dmx32, mcg_drs_t drs, void (*fllStableDelay)(void))

    CLOCK_SetInternalRefClkConfig(g_defaultClockConfigRun.mcgConfig.irclkEnableMode,
                                  g_defaultClockConfigRun.mcgConfig.ircs, g_defaultClockConfigRun.mcgConfig.fcrdiv);

    CLOCK_SetSimConfig(&g_defaultClockConfigRun.simConfig);

    SystemCoreClock = g_defaultClockConfigRun.coreClock;
}

Hope it can help you

BR

xiangjun Rong

0 件の賞賛
返信