Kinetisマイクロコントローラ・ナレッジ・ベース

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis Microcontrollers Knowledge Base

ディスカッション

ソート順:
1. Introduction MCUboot is a common used bootloader for most of Kinetis and i.mx RT devices. It can support download application via UART/USB/CAN/I2C/SPI. It enables quick and easy programming of Kinetis MCUs and i.mx RT MPU through the entire product life cycle, including application development, final product manufacturing, and beyond. K64 is a very popular device in Kinetis family. It has a M4 core, 512k and above flash, 120M main frequency and plenty of interface, such as I2C/SPI/UART/CAN/USB/ENET. But it is a bit awkward that the MCUboot demo of K64 is not include CAN. Does K64’s CAN can’t support bootloader application? No, of course not. Here we are going to port CAN function to K64 bootloader. There are two kind of CAN peripheral in Kinetis family, FlexCAN and MSCAN. FlexCAN is more complex than MSCAN. K64 has a FlexCAN. To speed up our work, we can port FlexCAN driver and related code from TWR-KV46 bootloader. Hardware: two TWR-SER board two sets of TWR-ELEV TWR-K65F150M TWR-K64F120M   Software: MCUXpresso 11.0 MCUBoot 2.0.0 package SDK_2.6.0_TWR-K64F120M 2. Software porting Step 1, copy below files to twrk64f120m_tower_bootloader project. \drivers\fsl_flexcan.c \drivers\fsl_flexcan.h        \source\bootloader\src\flexcan_peripheral_interface.c   Step 2, modify the project to enable the FlexCAN.       In bootloader_config.h, change BL_CONFIG_CAN definition to 1.        In peripherals_MK64F12.c, add #if BL_CONFIG_CAN     // CAN0     {.typeMask = kPeripheralType_CAN,      .instance = 0,      .pinmuxConfig = can_pinmux_config,      .controlInterface = &g_flexcanControlInterface,      .byteInterface = &g_flexcanByteInterface,      .packetInterface = &g_framingPacketInterface }, #endif    // BL_CONFIG_CAN       Pin mux setting. In peripherals_pinmux.h, add #define BL_ENABLE_PINMUX_CAN0 (BL_CONFIG_CAN) //! CAN pinmux configurations #define CAN0_RX_PORT_BASE PORTB #define CAN0_RX_GPIO_PIN_NUM 18             // PIN 13 in the PTA group #define CAN0_RX_FUNC_ALT_MODE kPORT_MuxAlt2 // ALT mode for CAN0 RX functionality for pin 13 #define CAN0_TX_PORT_BASE PORTB #define CAN0_TX_GPIO_PIN_NUM 19             // PIN 12 in the PTA group #define CAN0_TX_FUNC_ALT_MODE kPORT_MuxAlt2 // ALT mode for CAN0 TX functionality for pin 12       Set clock. FlexCAN clock source can be OSCERCLK or bus clock. Here we use bus clock run at 48Mhz. In flexcan_peripheral.c, add these code. const flexcan_timing_config_t bit_rate_table48m[] = {     { 23, 3, 4, 4, 4 }, /* 125 kHz */     { 11, 3, 4, 4, 4 }, /* 250 kHz */     { 5, 3, 4, 4, 4 },  /* 500 kHz */     { 3, 3, 4, 4, 4 },  /* 750 kHz */     { 2, 3, 4, 4, 4 }   /* 1   MHz */ }; change line 621 FLEXCAN_SetTimingConfig((CAN_Type *)baseAddr, &bit_rate_table48m[s_flexcanInfo.baudrate]); Step 3, compile the project.   3. Function test Software preparation To connect bootloader via CAN bus, NXP has TWR-K65 as bridge. But its source code is not in K64 SDK. It is in MCUBoot2.0.0 package. User can download the package from https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools/mcuboot-mcu-bootloader-for-nxp-microcontrollers:MCUBOOT The bridge project is called buspal which can be found in NXP_Kinetis_Bootloader_2_0_0\apps\bus_pal\MK65F18. BusPal is an embedded software tool that is available as a companion to blhost. The tool acts as a bus translator with an established connection with blhost over UART and with the target device over I2C, SPI, or CAN, and assists blhost in carrying out commands and responses from the USB target device. The BusPal is available for selected platforms. The source code for BusPal is provided with the Kinetis bootloader release, it support FRDM-KL25, TWR-KV46F150M and TWR-K65F180M and can be customized to run on other platforms. More detail of buspal is in Kinetis blhost User's Guide appendix C.   Hardware connection TWR-SER has TJA1050 as transceiver. We can connect J7 on both boards. When construct the Tower system, user should take care the power. The power tree is very flexible. Improper setting may cause TJA1050 can’t work.   The Buspal project on TWR-K65F180M use UART1 to connect with computer. The port is on TWR-SER. To make the connection simple, we can share the openSDA UART port. The openSDA UART use UART2, we can jump UART1 signal to J33 and J34 on K65 tower board.     Testing: Open a command window, type >blhost -p com4,57600 –buspal can,0,321,123 – get-property 10 This command can check if the whole system work properly. Then, you can download the code to K64 now. Please type >blhost -p com4,57600 –buspal can,0,321,123 – flash-image xxxxxx.s19 erase
記事全体を表示
1. AN5218-使用LPUART实现ISO7816接口功能​ 2. AN4373-Cookbook for SAR ADC Measuresments 3. AN5160-低功耗模式下使用UART唤醒Kinetis L系列MCU的方法​ 4. AN4905-Kinetis MCU 上支持无晶振 USB​ 5. AN3298-Kinetis芯片焊接温度曲线控制​ 6. AN5034-FleIO模拟UART​ 7. AN4752-FreeMaster的使用方法​ 8. AN4282-使用Kinetis的FlexMemory作为EEPROM的方法​ 9. AN4655-使用I2C接口引导更新Kinetis L系列MCU​ 10. AN4368-使用U盘方式更新带USB Host功能的Kinetis固件程序​
記事全体を表示
Freedog KL25Z | Linino The Freedog is a MIPS board based on the Atheros AR9331 and the Kinetis L Series KL25Z  MCUs built on ARM® Cortex™-M0+ processor. The Atheros processor supports Linino, a Linux distribution based on OpenWRT. The board has built-in Ethernet and WiFi support, a USB-A port, micro-SD card slot, 20 digital input/output pins (of which 7 can be used as PWM outputs and 12 as analog inputs), a 8 MHz crystal oscillator, a micro USB connection, an SWD header, and 3 reset buttons. The external row of the pin-header is Arduino compatible.
記事全体を表示
Test Environment: FRDM-KL43Z Rev. A MCUXpresso IDE v10.2.0 MCUXpresso SDK for FRDM-KL43Z V2.4.1(2018-06-18) Create new project in MCUXpresso IDE select [New project...], there will pop the SDK Wizard panel, then select [frdmkl43z]: Then, click [Next] will enter into [Configure the project] panel, we can set the [Project name] and select [flexio_i2s] in [driver]: Click [Finish], the new project was created. In general, the project is based on [hello_world] project with board default console available. In [Project Explorer], we could find the <fsl_flexio_i2s.c> & <fsl_flexio_i2s.h> & <fsl_flexio.c> & <fsl_flexio.h> files in drivers folder: Edit the code The application note AN5397 detailed introduce how FlexIO emulate I2S bus communication. The MCUXpresso SDK <flexio_i2s> driver using the AN5397 showed second solution to use two timers and two shifters. Please check here to get more detailed info. The I2S signal was below, we need to use four FlexIO pins to provide: BCLK, Fss, TxData & RxData. In <pin_mux.c> file, it need to config pin function, we use PTD7 pin provide I2S BCLK clock; PTD6 pin as I2S Frame_sync pin; PTD5 pin as Tx data pin; PTD6 pin as Rx data pin; In <frdmkl43z_flexio_i2s_interrupt_tx.c>,  config flexio_i2s and config the audio frame format: Please check attached source code for the detailed project info. Test result From the actual measured I2S signal, it shows the 8 bytes was sent out:
記事全体を表示
主板原理图。
記事全体を表示
Hello all,      So, this time there is a query on implementing IRDA communication by bit banging the GPIOs. So, I come up with an experiment to do so. Before that, why bit banging when KE02 supports IR communication right away by using FTM at TX and ACMP at RX? something similar to this Implementing infrared functions on UART0 with FRDM-KE02Z platform.        The answer lies in the waveform attached. In the code from the above discussion, the PWM modulation is performed on FTM channel for transmission, while the communication that customer required was different and the waveform required is the one attached.                                                                                           Note that the IRDA transmitter on FRDM-KE02Z is connected to UART0. But, in the attached code, UART0 is not configured for IRDA_TX. while ACMP is used for RX.      This post is intended to be a reference to those who want to implement IRDA with 3/16th bit width by bit banging.      Here is the schematic snapshot of the FRDM-KE02.   There are 2 sets of codes attached. 1. FRDM_KE02_singleboard_IRDA_BITBANGING_TX_RX - IRDA on a single board. 2. FRDM_KE02_interboard_IRDA_BITBANGING_TX_RX - IRDA between 2 boards.   To run a single board demo, the orientation of IRDA Transmitter and IRDA receiver is already taken care as both are on the same board. But, to run the second demo, the orientation is supposed to be something like this.   Both the demos are configured for 9600baud to communicate with PC. And the IRDA communication is at 2400baud.      The figure in page 13 of this document is referred while development. http://www.vishay.com/docs/82513/physical.pdf                                                                            Transmission - 1. The bit width is calculated depending on the required IRDA baud and PIT1 modulo is adjusted accordingly. There are 3 MOD values initialized one after the other to generate required IR frame. 2. The data to be transmitted is sent over the HyperTerminal @ 9600baud. This data is accordingly transmitted on PTB1.      The green waveform in the below oscilloscope snap is the IR frame from the above picture. The data being sent is 'e', the hex value of which is 0x65 which can be made out from the waveform. 0x65 is 0xa6 in reverse since LSB is sent out first in the IRDA protocol[The first logic high is the start bit. In IRDA transmission, logic low is data '1' and logic high is data '0'].                                                                                      Reception - 1. ACMP0 is configured to generate interrupts on either the rising edge or the falling edge. 2. The falling edge of the start bit triggers ACMP. 3. The logic received on PTA1 is decoded to arrive at the received data. 4. The falling edge on ACMP channel decides logic 0 and the PIT0 interrupt decides the logic 1.      The below waveform is the one probed at PTA1.                                                                     Thanks, Pramod TM
記事全体を表示
Kinetis L series MCUs combine the exceptional energy-efficiency and ease-of-use of the new ARM® Cortex™-M0+ processor with the performance, peripheral sets, enablement and scalability of the Kinetis 32-bit MCU portfolio. The Kinetis L series frees power-critical designs from 8- and 16-bit MCU limitations by combining excellent dynamic and stop currents with superior processing performance, a broad selection of on-chip flash memory densities and extensive analog, connectivity and HMI peripheral options. Kinetis L series MCUs are also hardware and software compatible with the ARM Cortex-M4-based Kinetis K series, providing a scalable migration path to more performance, memory and feature integration. The Kinetis L Series MCUs are Energy-Efficient Product Solutions by Freescale. For more information visit Freescale.com\Lseries
記事全体を表示
Hello Kinetis World, I just wanted to take this opportunity to share the press release for our newly announced WLCSP device.         http://finance.yahoo.com/news/thin-blade-grass-freescale-newest-120000684.html The Ultra Thin CSP, MK22FN512CBP12R, is equivalent to the standard height CSP, MK22FN512CBP12R.  Therefore, from Therefore, from a software enablement perspective, the MK22FN512CAP12 device can be selected as shown in the attached Processor Expert screenshot.  We're looking forward to seeing what amazing things you can accomplish using Kinetis technology!      
記事全体を表示
El programador USBDM es una interfaz de programación y depuración para los microcontroladores Freescale, existen varias versiones de esta herramienta, el programador MantaRay USBDM está basada en la versión para los microcontroladores HCS08(BDM) y Kinetis (SWDIO). Toda la información acerca de este proyecto puedes encontrarlo en http://usbdm.sourceforge.net/index.html BDM (Background debug mode) El puerto de programación BDM es una interfaz de programación desarrollada por Freescale para los microcontroladores HCS08 (8 bits) y Coldfire V1 (32 bits). Las características más sobresalientes sobre este puerto de programación es que solo utiliza un pin de programación (BKGD). Además de permitir la programación de la memoria flash, también permite el "debug in circuit" esto quiere decir que podemos depurar nuestro codigo en tiempo real a través del software Codewarrior. SWDIO Es la versión minima del JTAG para los microcontroladores Kinetis (Cortex ARM 32 bits) en la cual solo utiliza una linea de comunicación (SWDIO) y una señal de reloj (SWCLK). Este puerto esta en los Cortex M0 como son KL01, KL02, KL03, KL1x,KL2x,KE02,KE04 y KE06. El programador MantaRay USBDM permite la programación y la depuración de los microcontroladores de Freescale de la gama de 8 bits y 32 bits. Shrimp El complemento perfecto para el programador MantaRay USBDM es Shrimp, una pequeña tarjeta que tiene el tamaño exacta de un integrado con montaje DIP28 600mil, la cual, la hace una herramienta flexible, al hacer prototipos en una protoboard, y después en un prototipo final. La tarjeta Shrimp es compatible con los microcontroladores de 8 bits MC9S08PA16 y de 32 bits MKE02Z16, los dos totalmente compatibles en pines y periféricos. MC9S08PA16 8-Bit S08 central processor unit (CPU) – Up to 20 MHz bus at 2.7 V to 5.5 V across temperature range of -40 °C to 105 °C – Supporting up to 40 interrupt/reset sources – Supporting up to four-level nested interrupt – On-chip memory – Up to 16 KB flash read/program/erase over full operating voltage and temperature – Up to 256 byte EEPROM; 2-byte erase sector; program and erase while executing flash – Up to 2048 byte random-access memory (RAM) – Flash and RAM access protection MKE02Z16 • Operating characteristics – Voltage range: 2.7 to 5.5 V – Flash write voltage range: 2.7 to 5.5 V – Temperature range (ambient): -40 to 105°C • Performance – Up to 40 MHz ARM® Cortex-M0+ core and up to 20 MHz bus clock – Single cycle 32-bit x 32-bit multiplier – Single cycle I/O access port • Memories and memory interfaces – Up to 16 KB flash – Up to 256 B EEPROM – Up to 2 KB RAM Más información técnica la puedes encontrar en el siguiente link http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KE02&nodeId=01624698C90DE4 http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=S08P&nodeId=01624684491437EDDD Muy pronto mas adelantos de este proyecto
記事全体を表示
1.jicheng0622-AET-电子技术应用 2.wuyage-AET-电子技术应用 3.fanxi123-AET-电子技术应用
記事全体を表示
Hello Freedom community users Bheema has posted on the Element14 community a very clear tutorial (accessible following the link below) to create from scratch a basic project example featuring the SLCD of the FRDM-KL46Z with Processor Expert. Freescale Freedom development platform: [FRDM-K... | element14 Those steps should be very useful to create your own project featuring SLCD display and better understand the constraints of this peripheral. Happy SLCD Displaying Greg
記事全体を表示
This file describes how to install KSDK, is easy and simple with images and descriptions step by step, so you wont have problems with the installation.
記事全体を表示
On NXP website we had provide an application note " Kinetis-M Two-Phase Power Meter Reference Design" which can been found here: http://www.nxp.com/docs/en/application-note/DRM149.pdf  This is really a quite useful solution for 2-Phase Power Meter design. From the schematic, there has a LCD display. Many customer sent email to ask for the datasheet of this LCD display(GDH-1247WP). Yes agreed, it is really difficult to find it. ( Even from the google.) I am attaching the data sheet for the segment LCD here for customer to make reference.
記事全体を表示
Example of integrating CMSIS3.20 into MQX4.0.x on the TWR-K70F120M (with floating point unit) using CW10.4 using the MQX4.0.2\mqx\examples\hello2 project. In the attached ZIP file (hello2twrk70f120m_CMSIS_FPU.zip) is a MSWord document detailing the steps used.  That document name is TWR-K70F120M_CMSIS_CW10.4_MQX4.0.x.docx. Regards, David
記事全体を表示
1. Overview BLE beacon is a common use of low power Bluetooth and it broadcasts advertisement at some interval. Freescale BLE beacon demo use Freescale Kinetis KL16 low power MCU and EMC EM9301 Bluetooth controller to implement a beacon reference design. Freescale BLE beacon features low power consumption of an average cost of 50uA with 600ms interval. Freescale Kinetis KL16 coordinates with EM9301 through SPI interface. View attachment to learn more
記事全体を表示
Hi Team :      We are working on KSDK project recently . I would like to share an experience to migrate a project to a new device that is not listed in KSDK . I hope that helpful . Best regards, David
記事全体を表示
Freescale Semiconductor is to demonstrate its Kinetis L series microcontrollers (MCUs) built on the ARM Cortex-M0+ processor at DESIGN West in San Jose, California, with alpha sampling due to start in the second quarter of 2012. Freescale  says the ability to demonstrate these devices is possible due to its  close partnership between ARM during the Cortex-M0+ core development  process and as a lead partner provided  input that helped ARM define and  develop the processor. The devices are slated for applications  such as domestic appliances, portable medical systems, smart meters,  lighting, power and motor control systems. "Our close partnership  with ARM throughout the design and development of their new core has  positioned us as the first MCU supplier to produce and demonstrate an MCU based on the Cortex-M0+ and continues our strategy of driving to  market new products based on the ARM architecture," said Reza  Kazerounian, senior vice president and general manager of Freescale’s  Automotive, Industrial and Multi-Market Solutions Group. Mike  Inglis, executive vice president and general manager of ARM’s Processor  Division, added "With the addition of the L series to their Kinetis  line, Freescale is creating one of the industry’s broadest, most  scalable ARM Cortex-M MCU portfolios, ranging from very low-cost,  entry-level products based on the ARM Cortex-M0+ processor, up to 4 MB,  200 MHz devices based on the Cortex-M4 processor." Manufactured  using Freescale’s low-leakage, 90 nm thin film storage (TFS) process  technology, the Kinetis L series will have a selection of on-chip flash  memory densities and analog, connectivity and HMI peripheral options. Upward  migration through the Kinetis portfolio is available via compatible Kinetis K series devices (built on the ARM Cortex-M4 processor) that  provide access to DSP performance and advanced feature integration. The  ARM Cortex-M0+ processor includes a reduced two-stage pipeline,  allowing faster branch instruction execution, single-cycle access to I/O  and critical peripherals, optimized access to program memory, linear 4  GB address space that removes the need for paging, reducing software  complexity and ensuring a more 8-bit-like user experience and a micro  trace buffer, providing a low-cost trace solution that allows faster bug  identification and correction without the need for additional I/O  resources. Freescale will demonstrate the ARM Cortex-M0+ core at its exhibition booth #1604 at DESIGN West , March 26-29 at the San Jose McEnery Convention Center.
記事全体を表示
Today the universal motor is still widely used in home appliances such as vacuum cleaners, washers, hand tools, and food processors. The operational mode, which is used in this application, is closed loop and regulated speed. This mode requires a speed sensor on the motor shaft. Such a sensor is usually an incremental sensor or a tachometer generator. The kind of motor and its drive have a high impact on many home appliance features like cost, size, noise, and efficiency. Electronic control is usually necessary when variables speed or energy savings are required. MCUs offer the advantages of low cost and attractive design. They can operate with only a few external components and reduce the energy consumption as well as the cost. This circuit was designed as a simple schematic using key features of a Kinetis L MCU. For demonstration purposes, the Freescale low cost Freedom KL25z development platform was used. This application note describes the design of a low-cost phase angle motor control drive system based on Freescales’s Kinetis L series microcontroller (MCU) and the MAC4DC snubberless triac. The low-cost single-phase power board is dedicated for universal brushed motors operating from 1000 RPMs to 15,000 RPMs. This application note explains both HW and SW design with an ARM Kinetis L series MCU. Such a low-cost MCU is powerful enough to do the whole job necessary for driving a closed loop phase angle system as well as many others algorithms.        -Freedom development platform with universal motor drive board extension The phase angle control technique is used to adjust the voltage applied to the motor. A phase shift of the gate’s pulses allows the effective voltage, seen by the motor, to be varied. All required functions are performed by just one integrated circuit and a small number of external components. This allows a compact printed circuit board (PCB) design and a cost-effective solution. Learn more about the Kinetis L series Freedom Board Get the full application note in the link bellow:
記事全体を表示
Recently, some customers have provided us with feedback stating they have been experiencing difficulties when connecting  Kinetis L series  microcontrollers using Multilink Universal probes, after checking the connection and software settings no obvious errors could be found. This recurrent problem has been confirmed by several customers, the  problem is caused by a long connection line. My suggestion is to keep connection line length to 10cm or less; otherwise, the IDE may not be able to establish the connection through the Multilink Universal.
記事全体を表示
New 32-bit MCUs designed to transform consumer and industrial applications currently using legacy 8- and 16-bit architectures SAN ANTONIO, Jun 19, 2012 (BUSINESS WIRE) -- Freescale Semiconductor FSL +0.80% is now offering alpha samples of its Kinetis L series, the industry's first microcontrollers (MCUs) built on the  ARM(R) Cortex(TM)-M0+ processor. Kinetis L series devices are on display this week at the Freescale        Technology Forum (FTF) Americas and were demonstrated during the event's opening keynote address. As machine-to-machine communication expands and network connectivity  becomes ubiquitous, many of today's standalone, entry-level applications will require more intelligence and functionality. With the Kinetis  L series , Freescale provides the ideal opportunity for users of legacy 8- and 16-bit architectures to migrate to 32-bit platforms and bring additional intelligence to everyday devices without increasing power  consumption and cost or sacrificing space. Applications, such as small  appliances, gaming accessories, portable medical systems, audio systems, smart meters, lighting and power control, can now leverage 32-bit capabilities and the scalability needed to expand future product lines -- all at 8- and 16-bit price and power consumption levels. "In our view, 8- and 16-bit development has reached the end of the road. Those architectures simply can't keep up as the Internet of Things gains traction," said Geoff Lees, vice president and general manager of Freescale's Industrial & Multi-Market MCU business. "Kinetis L series MCUs are ideal for the new wave of connected applications, combining the required energy efficiency, low price, development ease and small  footprint with the enhanced performance, peripherals, enablement and scalability of the Kinetis 32-bit portfolio." Extreme energy efficiency The ARM Cortex-M0+ processor consumes approximately one-third of the energy of any 8- or 16-bit processor available today, while delivering  between two to 40 times more performance. The Kinetis L series supplements the energy efficiency of the core with the latest in  low-power MCU platform design, operating modes and energy-saving peripherals. The result is an MCU that consumes just 50 uA/MHz* in very-low-power run (VLPR) mode and can rapidly wake from a reduced power state, process data and return to sleep, extending application battery life. These advantages are demonstrated in the FTF demo, which compares the energy-efficiency characteristics of the Kinetis L series against solutions from Freescale competitors in a CoreMark benchmark analysis.        The Kinetis L series is also part of the Freescale Energy-Efficient Solutions program. Kinetis L series energy-saving peripherals do more with less power by maintaining functionality even when the MCU is in deep sleep modes. In traditional MCUs, the main clock and processor core must be activated to perform even trivial tasks such as sending or receiving data, capturing or generating waveforms or sampling analog signals. Kinetis L series peripherals are able to perform these functions without involving the core or main system, drastically reducing power consumption and improving battery life. Built using Freescale's innovative, award-winning flash memory technology, the Kinetis L series offers the industry's lowest-power flash memory implementation. This improves upon the conventional silicon-based charge storage approach by creating nano-scale silicon islands to store charge instead of using continuous film, improving the flash memory's immunity to typical sources of data loss. "The Internet of Things needs very low-cost, low-power processors that        can deliver good performance," said Tom R. Halfhill, a senior analyst        with The Linley Group and senior editor of Microprocessor Report. "As  the first 32-bit microcontrollers to use ARM's Cortex-M0+ processor core, Freescale's Kinetis L-series MCUs will bring the energy efficiency and prices typically associated with 8- and 16-bit MCUs to a broad range of consumer and industrial applications." Development simplicity The Kinetis L series addresses the ease-of-use requirement critical for entry-level developers through innovations including: -- The Freescale Freedom development platform, a small, low-power, cost-efficient evaluation and development system for quick application prototyping and demonstration. It combines an industry-standard form factor with a rich set of third-party expansion board options. An integrated USB debug interface offers an easy-to-use mass-storage device mode flash programmer, a virtual serial port and classic programming and run-control capabilities. -- Processor Expert software, a GUI-based, device-aware software generation tool that eliminates the need to write peripheral start-up code or device drivers. Helps developers easily migrate from 8- and 16-bit to 32-bit solutions by simplifying the software architecture and  dramatically reducing application development time. --  The Kinetis MCU Solution Advisor, a web-based application with an interactive MCU product selector that helps identify the best-suited MCU by applying dynamic filters based on operating characteristics, packaging options, memory configuration and peripheral hardware library. Integration and scalability Each Kinetis L series family includes scalable flash memory options, pin-counts and analog, communication, timing and control peripherals, providing easy migration paths for end product line expansion. Features common to the Kinetis L series families include: --         48 MHz ARM Cortex-M0+ core --         High-speed 12/16-bit analog-to-digital converters --         12-bit digital-to-analog converters --         High-speed analog comparators --         Low-power touch sensing with wake-up on touch from reduced power states --         Powerful timers for a broad range of applications including motor control The first three Kinetis L series families: --         Kinetis L0 family -- the entry point into the Kinetis L series. Includes eight to 32 KB of flash memory and ultra-small 4mm x 4mm QFN packages. Pin-compatible with the Freescale 8-bit S08P family. Software- and tool-compatible with all other Kinetis L series families. --         Kinetis L1 family -- with 32 to 256 KB of flash memory and  additional communications and analog peripheral options. Compatible with the Kinetis K10 family. --         Kinetis L2 family -- adds USB 2.0 full-speed host/device/OTG. Compatible with the Kinetis K20 family. The Kinetis L series is pin- and software-compatible with the Kinetis  K series (built on the ARM Cortex-M4 processor), providing a migration path to DSP performance and advanced feature integration. Availability and pricing Kinetis L series alpha samples are available now, with broad market sample and tool availability planned for Q3. Pricing starts at a suggested resale price of 49 cents (USD) in 10,000-unit quantities. The Freescale Freedom development platform is planned for Q3 availability at  a suggested resale price of $12.95 (USD). For more information about Kinetis L series MCUs, visit   www.freescale.com/Kinetis/Lseries    . *Typical current at 25C, 3V supply, for Very Low Power Run at 4MHz core  frequency, 1MHz bus frequency running code from flash with all peripherals off. About the Freescale Technology Forum Created to drive innovation and collaboration, the Freescale Technology Forum (FTF) has become one of the developer events of the year for the embedded systems industry. The Forum has drawn more than 48,000 attendees at FTF events worldwide since its inception in 2005. Our annual flagship event, FTF Americas, takes place June 18-21, 2012, in San Antonio, Texas. About Freescale Semiconductor Freescale Semiconductor  FSL +0.80% is a global leader in embedded processing solutions, providing industry leading products that are advancing the automotive, consumer, industrial and networking markets. From microprocessors and microcontrollers to sensors, analog integrated  circuits and connectivity -- our technologies are the foundation for the innovations that make our world greener, safer, healthier and more connected. Some of our key applications and end-markets include automotive safety, hybrid and all-electric vehicles, next generation wireless infrastructure, smart energy management, portable medical  devices, consumer appliances and smart mobile devices. The company is  based in Austin, Texas, and has design, research and development,        manufacturing and sales operations around the world.   www.freescale.com Freescale, the Freescale logo, Energy Efficient Solutions logo, Kinetis  and Processor Expert are trademarks of Freescale Semiconductor, Inc.,  Reg. U.S. Pat. & Tm. Off. ARM is the registered trademark of ARM  Limited. Cortex is the trademark of ARM Limited. All other product or  service names are the property of their respective owners. (C) 2012   Freescale Semiconductor, Inc. Photos/Multimedia Gallery Available:   http://www.businesswire.com/cgi-bin/mmg.cgi?eid=50313420&lang=en SOURCE: Freescale Semiconductor
記事全体を表示